AOSP build failed :Android 11 with imx8qxpC0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AOSP build failed :Android 11 with imx8qxpC0

2,061 Views
jackey267
Contributor II

hello NXP : 

1 another try to build AOSP (Android 11)has been failed: 

2 the follow was the error log file for your reference: 

3  failed at location: 

[ 99% 136548/137181] Target Java: out/target/common/obj/APPS/Dialer_intermediates/classes-full-debug.jar
FAILED: out/target/common/obj/APPS/Dialer_intermediates/classes-full-debug.jar

4  more detailed please decompress the zip log file to see it .

5 hope to hear from you !

6 thank you for your help. 

7 ubuntu20.04.3 LTS +Intel(R) Core(TM) i7-10700 CPU @ 2.90GHz 16Ghz +MemTotal: 16169652 kB 

8 cmd  : 

$source ~/imx-android-11.0.0_2.2.0/imx_android_setup.sh

$cd ~/tools 

$git clone https://android.googlesource.com/platform/prebuilts/clang/host/linux-x86  prebuilt-android-clang -b master

$export CLANG_PATH=/home/zsh/tools/prebuilt-android-clang

$export AARCH64_GCC_CROSS_COMPILE=/opt/gcc-arm-8.3-2019.03-x86_64-aarch64-elf/bin/aarch64-elf-

:~/android_build$ source build/envsetup.sh
:~/android_build$ lunch mek_8q-eng 

$./imx-make.sh -j16 2>&1 | tee build-log.txt 

 

9 yesterday night it was failed one more time .build-log_4.zip thanks .10.25th,9:19am shenzhen china .thanks .

0 Kudos
Reply
1 Reply

2,039 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

11_2.2 doesn't support qxp,android111_1.0.0 is lastest version for qxp

 

 

2 Supported Hardware SoC/Boards
The supported hardware system-on-chip (SoCs)/boards are listed as follows:
• i.MX 8M Mini EVK
Supported daughter boards:
— With DDR4 RAM, Rohm bd71847 PMIC chip and Cypress CYW43455 Wi-Fi/Bluetooth module
— With LPDDR4 RAM, NXP pca9450 PMIC chip and NXP 88W8987 Wi-Fi/BT module.
Supported mother board:
— Rev. C mother board
• i.MX 8M Nano EVK
Supported daughter boards:
— With DDR4 RAM, Rohm bd71847 PMIC chip and Cypress CYW43455 Wi-Fi/Bluetooth module
— With LPDDR4 RAM, NXP pca9450 PMIC chip and NXP 88W8987 Wi-Fi/Bluetooth module
Supported mother board:
— Rev. C mother board
• i.MX 8M Plus (Silicon Revision A1) EVK Board and Platform
• i.MX 8M Quad EVK Rev. A Board and Platform

 

 

 

0 Kudos
Reply