AN12195 build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,026件の閲覧回数
Enuwai
Contributor III

AN12195 has the following build related items
  5.1.2. Setup aarch64 toolchain
  5.1.3. Build uboot-imx and copy binaries
  5.1.4. Apply low-power patch and build bl31.bin
  5.1.5. Unpack binary firmware
  5.1.6. Build final flash.bin
  5.2. Rebuild kernel with new drivers

If I don't build all of these, won't the playback/recording sample programs in this application note work?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,967件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
5 返答(返信)
3,008件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what bsp version did you test? did you test on imx8mq evk board, right?

0 件の賞賛
返信
2,999件の閲覧回数
Enuwai
Contributor III

Hi Joanxie,

> what bsp version did you test?
The version is 4.9.51.

> did you test on imx8mq evk board, right?
Yes, I plan to run imx8mq evk, but the build will not pass.
I have already asked the NXP community about the items that are not building successfully.
Here, these are questions about whether all of the above should be built.

 

0 件の賞賛
返信
2,974件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

these are questions about whether all of the above should be built.

> what do you mean? what items do you want to build? pls give me more detailed information

0 件の賞賛
返信
2,971件の閲覧回数
Enuwai
Contributor III

I just want to run the playback/recording sample program in the application note.
It is necessary to build all the items written at the top, right?

0 件の賞賛
返信
2,968件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes, correct

0 件の賞賛
返信