Hi,
We are working with ADV7181C to get video from SVGA PC output (800x600@60Hz). The CSI is connected through :
CSIx_DAT4 ~ CSIx_DAT9
CSIx_DAT12 ~ CSIx_DAT19
We have set ADV7181C register's properly to output 16-bit YUV 4:2:2 as follow :
Then we applied patch from https://community.freescale.com/docs/DOC-97981.
But when we try to get frames with the following command :
~# ./mxc_v4l2_capture_sgrbg8 -ow 800 -oh 600 -c 500 -fr 25 testsgrbg8.bin
in_width = 176, in_height = 144
out_width = 800, out_height = 600
top = 0, left = 0
sensor chip is adv7180_decoder
sensor supported frame size:
720x576
Width = 800 Height = 600 Image size = 960000
pixelformat: GRBG
VIDIOC_DQBUF failed.
VIDIOC_QBUF failed
We get timeout error (complete log) :
Jan 16 17:07:35 imx6q user.debug kernel: In MVC: mxc_v4l_open
Jan 16 17:07:35 imx6q user.debug kernel: device name is Mxc Camera
Jan 16 17:07:35 imx6q user.debug kernel: adv7180 2-0021: adv7180:ioctl_g_ifparm
Jan 16 17:07:35 imx6q user.debug kernel: adv7180 2-0021: adv7180:ioctl_g_fmt_cap
Jan 16 17:07:35 imx6q user.debug kernel: Returning size of 720x625
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l_open: v2f pix widthxheight 800 x 600
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l_open: crop_bounds widthxheight 720 x 625
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l_open: crop_defrect widthxheight 720 x 625
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l_open: crop_current widthxheight 720 x 625
Jan 16 17:07:35 imx6q user.debug kernel: On Open: Input to ipu size is 720 x 625
Jan 16 17:07:35 imx6q user.debug kernel: adv7180 2-0021: In adv7180:ioctl_init
Jan 16 17:07:35 imx6q user.debug kernel: adv7180 2-0021: adv7180:ioctl_dev_init
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_DBG_G_CHIP_IDENT chip_ident=7180, revision=0x0
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_ENUM_FRAMESIZES index=0, pixelformat=@��*, type=0 Mxc Camera: - Unknown type!
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_ENUM_FRAMESIZES index=1, pixelformat=@�ﴴ*, type=0 Mxc Camera: - Unknown type!
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_ENUM_FRAMESIZES error -22
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_ENUM_FMT error -22
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_S_PARM type=1
Jan 16 17:07:35 imx6q user.debug kernel: In mxc_v4l2_s_param
Jan 16 17:07:35 imx6q user.debug kernel: adv7180 2-0021: In adv7180:ioctl_g_parm
Jan 16 17:07:35 imx6q user.debug kernel: type is V4L2_BUF_TYPE_VIDEO_CAPTURE
Jan 16 17:07:35 imx6q user.debug kernel: Current capabilities are 0
Jan 16 17:07:35 imx6q user.debug kernel: Current capturemode is 0 change to 0
Jan 16 17:07:35 imx6q user.debug kernel: Current framerate is 30 change to 25
Jan 16 17:07:35 imx6q user.debug kernel: adv7180 2-0021: In adv7180:ioctl_s_parm
Jan 16 17:07:35 imx6q user.debug kernel: adv7180 2-0021: adv7180:ioctl_g_ifparm
Jan 16 17:07:35 imx6q user.debug kernel: clock_curr=mclk=27000000
Jan 16 17:07:35 imx6q user.debug kernel: adv7180 2-0021: adv7180:ioctl_g_fmt_cap
Jan 16 17:07:35 imx6q user.debug kernel: Returning size of 720x625
Jan 16 17:07:35 imx6q user.debug kernel: g_fmt_cap returns widthxheight of input as 720 x 625
Jan 16 17:07:35 imx6q user.debug kernel: csi params :
Jan 16 17:07:35 imx6q user.debug kernel: clock_mode 0x0
Jan 16 17:07:35 imx6q user.debug kernel: fmt 0x47425247
Jan 16 17:07:35 imx6q user.debug kernel: width 0x9
Jan 16 17:07:35 imx6q user.debug kernel: ext_vsync 0x1
Jan 16 17:07:35 imx6q user.debug kernel: vsync_pol 0x0
Jan 16 17:07:35 imx6q user.debug kernel: hsync_pol 0x0
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_S_INPUT value=0
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_G_CROP type=vid-cap
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: Rect start at 0x0, size=720x625
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_S_CROP type=vid-cap
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: Rect start at 0x0, size=176x144
Jan 16 17:07:35 imx6q user.debug kernel: Cropping Input to ipu size 176 x 144
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_S_FMT type=vid-cap
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: width=800, height=600, format=GRBG, field=unknown, bytesperline=800 sizeimage=0, colorspace=2132
Jan 16 17:07:35 imx6q user.debug kernel: In MVC: mxc_v4l2_s_fmt
Jan 16 17:07:35 imx6q user.debug kernel: type=V4L2_BUF_TYPE_VIDEO_CAPTURE
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l2_s_fmt: v2f pix widthxheight 800 x 600
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l2_s_fmt: crop_bounds widthxheight 720 x 625
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l2_s_fmt: crop_defrect widthxheight 720 x 625
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l2_s_fmt: crop_current widthxheight 176 x 144
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_S_CTRL id=0x8000000, value=0
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_v4l2_s_ctrl
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_streamoff
Jan 16 17:07:35 imx6q user.debug kernel: MVC: In mxc_free_frame_buf
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_allocate_frame_buf - size=960000
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_REQBUFS count=3, type=vid-cap, memory=mmap
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_G_FMT type=vid-cap
Jan 16 17:07:35 imx6q user.debug kernel: In MVC: mxc_v4l2_g_fmt type=1
Jan 16 17:07:35 imx6q user.debug kernel: type is V4L2_BUF_TYPE_VIDEO_CAPTURE
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l2_g_fmt: v2f pix widthxheight 800 x 600
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l2_g_fmt: crop_bounds widthxheight 720 x 625
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l2_g_fmt: crop_defrect widthxheight 720 x 625
Jan 16 17:07:35 imx6q user.debug kernel: End of mxc_v4l2_g_fmt: crop_current widthxheight 176 x 144
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: width=800, height=600, format=GRBG, field=unknown, bytesperline=1600 sizeimage=960000, colorspa2
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_v4l2_buffer_status
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_QUERYBUF 00:00:00.00000000 index=0, type=vid-cap, flags=0x00000001, field=0, sequence=0,p
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: bytesused=0, offset/userptr=0x18800000, length=962560
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_mmap
Jan 16 17:07:35 imx6q user.debug kernel: pgoff=0x18800, start=0x2ad7d000, end=0x2ae68000
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_v4l2_buffer_status
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_QUERYBUF 00:00:00.00000000 index=1, type=vid-cap, flags=0x00000001, field=0, sequence=0,p
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: bytesused=0, offset/userptr=0x18b00000, length=962560
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_mmap
Jan 16 17:07:35 imx6q user.debug kernel: pgoff=0x18b00, start=0x2aeb9000, end=0x2afa4000
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_v4l2_buffer_status
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_QUERYBUF 00:00:00.00000000 index=2, type=vid-cap, flags=0x00000001, field=0, sequence=0,p
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: bytesused=0, offset/userptr=0x18c00000, length=962560
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_mmap
Jan 16 17:07:35 imx6q user.debug kernel: pgoff=0x18c00, start=0x2b097000, end=0x2b182000
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_QBUF 00:00:00.00000000 index=0, type=vid-cap, flags=0x00000003, field=0, sequence=0, memp
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: bytesused=0, offset/userptr=0x18800000, length=0
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_QBUF 00:00:00.00000000 index=1, type=vid-cap, flags=0x00000003, field=0, sequence=0, memp
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: bytesused=0, offset/userptr=0x18b00000, length=0
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_QBUF 00:00:00.00000000 index=2, type=vid-cap, flags=0x00000003, field=0, sequence=0, memp
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: bytesused=0, offset/userptr=0x18c00000, length=0
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000
Jan 16 17:07:35 imx6q user.debug kernel: Mxc Camera: VIDIOC_STREAMON type=vid-cap
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_streamon
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: init channel = 15
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: initializing idma ch 0 @ c08c0000
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: ch 0 word 0 - 00000000 00000000 00000000 E0001800 00095C63
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: ch 0 word 1 - 031A0000 00634000 00C1C000 00018FC0 00000000
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: PFS 0x6,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: BPP 0x3,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: NPB 0x7
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: FW 799,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: FH 599,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: EBA0 0x18d00000
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: EBA1 0x18d00000
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: Stride 1599
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: scan_order 0
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: uv_stride 0
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: u_offset 0x0
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: v_offset 0x0
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: Width0 0+1,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: Width1 0+1,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: Width2 0+1,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: Width3 0+1,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: Offset0 0,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: Offset1 0,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: Offset2 0,
Jan 16 17:07:35 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: Offset3 0
Jan 16 17:07:35 imx6q user.debug kernel: In MVC:mxc_v4l_dqueue
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
Jan 16 17:07:45 imx6q user.err kernel: ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
Jan 16 17:07:45 imx6q user.debug kernel: Mxc Camera: VIDIOC_DQBUF error -62
Jan 16 17:07:45 imx6q user.err kernel: ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued
Jan 16 17:07:45 imx6q user.debug kernel: Mxc Camera: VIDIOC_QBUF error -22
Jan 16 17:07:45 imx6q user.debug kernel: Mxc Camera: VIDIOC_STREAMOFF type=vid-cap
Jan 16 17:07:45 imx6q user.debug kernel: In MVC:mxc_streamoff
Jan 16 17:07:45 imx6q user.debug kernel: imx-ipuv3 imx-ipuv3.0: CSI stop timeout - 5 * 10ms
Jan 16 17:07:45 imx6q user.debug kernel: In MVC:mxc_free_frames
Jan 16 17:07:45 imx6q user.debug kernel: In MVC:mxc_v4l_close
Jan 16 17:07:45 imx6q user.debug kernel: In MVC:mxc_streamoff
Jan 16 17:07:45 imx6q user.debug kernel: mxc_v4l_close: release resource
Jan 16 17:07:45 imx6q user.debug kernel: MVC: In mxc_free_frame_buf
Jan 16 17:07:45 imx6q user.debug kernel: In MVC:mxc_free_frames
Here is setting from adv7180.c ioctl_g_ifparm() :
/* Initialize structure to 0s then set any non-0 values. */ | |
memset(p, 0, sizeof(*p)); | |
p->if_type = V4L2_IF_TYPE_BT656; /* This is the only possibility. */ | |
p->u.bt656.mode = V4L2_IF_TYPE_BT656_MODE_NOBT_8BIT; | |
p->u.bt656.bt_sync_correct = 1; | |
//p->u.bt656.nobt_hs_inv = 1; | |
//p->u.bt656.nobt_vs_inv = 1; | |
p->u.bt656.clock_curr = 27000000; //Gated clock mode | |
/* ADV7180 has a dedicated clock so no clock settings needed. */ |
Hi kamel
for ADV7180/bt656 one needs to use mxc_v4l2_tvin, also
one can look at below activities
https://community.freescale.com/message/314760#314760
Re: ADV7180 on IMX6 giving magenta output
Best regards
igor
Hi Igor,
Im using mxc_v4l2_capture to because tvin doesn't have redirection to binary file, only display on framebuffer is supported.
We have both adv7180 and adv7181c, the first work well with default bt656 mode with a cvbs input but with adv7181c, we need to capture a svga/xvga input so we can't configure adv7181c with bt656 (look at SDP vs CP).
Is there any application note on how to properly set csi with 16-bit generic data ? What configuration should I have in registers CSI0_SENS_CONF, CSI0_SENS_FRM_SIZE, CSI0_ACT_FRM_SIZE and CPMEM ?
There is a lot of discussion but no one gives a correct answer or scheme to follow ?
Hi kamel
I am afraid there are no such documents, link below is for
16-bit generic data
https://community.freescale.com/message/331888
https://community.freescale.com/message/309833#309833
~igor