ACC conformance test FAILED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ACC conformance test FAILED

10,771 Views
pyraohms
Contributor III

Trying to build my first image using Yocto. The compiler fails in the following step:

| checking whether your compiler passes the ACC conformance test... FAILED
| configure:
| configure: Your compiler failed the ACC conformance test - for details see
| configure: `config.log'. Please check that log file and consider sending
| configure: a patch or bug-report to <[email protected]>.
| configure: Thanks for your support.
| configure:
| configure: error: ACC conformance test failed. Stop.
| NOTE: The following config.log files may provide further information.
| WARNING: exit code 1 from a shell command.
| NOTE: /home/per/fsl-release-bsp/builds/tmp/work/x86_64-linux/lzop-native/1.03-r0/build/config.log
| ERROR: configure failed
| ERROR: Function failed: do_configure (log file is located at /home/per/fsl-release-bsp/builds/tmp/work/x86_64-linux/lzop-native/1.03-r0/temp/log.do_configure.25098)
ERROR: Task 402 (virtual:native:/home/per/fsl-release-bsp/sources/poky/meta/recipes-support/lzop/lzop_1.03.bb, do_configure) failed with exit code '1'

Can anyone offer a suggestion of how this may be solved?

Thanks

2 Replies

6,254 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply

6,254 Views
pyraohms
Contributor III

The problem can be solved by replacing the contents of <yocto>/sources/poky/meta/recipes-support/lzop/lzop/x32_abi_miniacc_h.patch with the following:

Fix get of FLAGS register in x32 ABI,

x32 ABI requires to have 64-bit variable to store FLAGS register
instead of size_t that is 32-bit variable, this fix operand
type mismatch when try to pop previous pushf value.

Upstream-Status: Submitted

Signed-off-by: Aníbal Limón <[email protected]>

Index: lzop-1.03/src/miniacc.h
===================================================================
--- lzop-1.03.orig/src/miniacc.h
+++ lzop-1.03/src/miniacc.h
@@ -754,6 +754,9 @@
#elif defined(__amd64__) || defined(__x86_64__) || defined(_M_AMD64)
# define ACC_ARCH_AMD64 1
# define ACC_INFO_ARCH "amd64"
+# if defined(__ILP32__)
+# define ACC_ARCH_AMD64_X32 1
+# endif
#elif defined(__thumb__) || (defined(_M_ARM) && defined(_M_THUMB))
# define ACC_ARCH_ARM 1
# define ACC_ARCH_ARM_THUMB 1
@@ -4469,12 +4469,12 @@
#if defined(__MSDOS__) && defined(__TURBOC__) && (__TURBOC__ < 0x0150)
#elif 1 && (ACC_CC_SUNPROC) && !defined(ACCCHK_CFG_PEDANTIC)
#else
- ACCCHK_ASSERT((1 << (8*SIZEOF_INT-1)) < 0)
+ ACCCHK_ASSERT((int)(1u << (8*SIZEOF_INT-1)) < 0)
#endif
ACCCHK_ASSERT((1u << (8*SIZEOF_INT-1)) > 0)
#if 1 && (ACC_CC_SUNPROC) && !defined(ACCCHK_CFG_PEDANTIC)
#else
- ACCCHK_ASSERT((1l << (8*SIZEOF_LONG-1)) < 0)
+ ACCCHK_ASSERT((long)(1ul << (8*SIZEOF_LONG-1)) < 0)
#endif
ACCCHK_ASSERT((1ul << (8*SIZEOF_LONG-1)) > 0)
#if defined(acc_int16e_t)
@@ -4703,7 +4703,7 @@
#elif 1 && (ACC_CC_LCC || ACC_CC_LCCWIN32) && !defined(ACCCHK_CFG_PEDANTIC)
#elif 1 && (ACC_CC_SUNPROC) && !defined(ACCCHK_CFG_PEDANTIC)
#elif !(ACC_BROKEN_INTEGRAL_PROMOTION) && (SIZEOF_INT > 1)
- ACCCHK_ASSERT( (((unsigned char)128) << (int)(8*sizeof(int)-8)) < 0)
+ ACCCHK_ASSERT( (int)((unsigned int)((unsigned char)128) << (int)(8*sizeof(int)-8)) < 0)
#endif
#if (ACC_CC_BORLANDC && (__BORLANDC__ >= 0x0530) && (__BORLANDC__ < 0x0560))
# pragma option pop
@@ -6787,7 +6790,11 @@ ACCLIB_PUBLIC_NOINLINE(void, acc_debug_n
ACCLIB_PUBLIC_NOINLINE(int, acc_debug_align_check_query) (void)
{
#if (ACC_ARCH_AMD64 || ACC_ARCH_I386) && (ACC_ASM_SYNTAX_GNUC)
+# if defined(ACC_ARCH_AMD64_X32)
+ unsigned long long r;
+# else
size_t r;
+# endif
__asm__ __volatile__("pushf\n pop %0\n" : "=a" (r) : : __ACC_ASM_CLOBBER);
return (int)(r >> 18) & 1;
#elif (ACC_ARCH_I386) && (ACC_ASM_SYNTAX_MSC)

Above is a concatenation of the original contentes of the file with the patch found here:

openembedded-core/lzop-1.03-gcc6.patch at master · openembedded/openembedded-core · GitHub 

It can surely be done in a nicer way, but i do not know how. This made it work for me though!