About imx6dl hdmi cec and hpd(hotplug detection) question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About imx6dl hdmi cec and hpd(hotplug detection) question

跳至解决方案
1,698 次查看
yenchao
Contributor IV

Hi All,

I'm working on imx6dl android 5.1(kernel 3.14.52) and have a question on hdmi cec and hpd(hotplug detection).

That is when a monitor send hpd(hotplug detection) low to our board.

Our board won't receive any hdmi cec signal until we re-initilaize hdmi cec function.

I know it is reasonable for not receiving hdmi cec signal when board receive hpd low.
But I am curious to know why this happen?

Is there any register that will disable hdmi cec signal when board receive hpd low?

Any thoughts or suggestions will be greatly appreciated.

Thx

Yen

标签 (4)
0 项奖励
回复
1 解答
1,392 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yen

one can check sect.33.5.219 PHY RXSENSE, PLL lock, and HPD Status Register
(HDMI_PHY_STAT0), sect.33.5.221 PHY RXSENSE, PLL lock, and HPD Mask Register
(HDMI_PHY_MASK0) i.MX6DQ Reference Manual
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,393 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yen

one can check sect.33.5.219 PHY RXSENSE, PLL lock, and HPD Status Register
(HDMI_PHY_STAT0), sect.33.5.221 PHY RXSENSE, PLL lock, and HPD Mask Register
(HDMI_PHY_MASK0) i.MX6DQ Reference Manual
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复