What is maximun resolution that i.MX6 Dual can manage with MiPi DSI?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is maximun resolution that i.MX6 Dual can manage with MiPi DSI?

ソリューションへジャンプ
1,540件の閲覧回数
jdepedro
Contributor IV

 Looking at the NXP documentation there is a mismatching or a typo, looking at the manuals:

"Programmable display resolutions, from 160x120(QQVGA) to 1280x720(XVGA)."

"Programmable display resolutions, from 160x120(QQVGA) to 1024x768(XVGA)"

Also seems like XVGA is not an standard format: wikipedia

Could you confirm what is the correct information? Thanks

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,265件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  "The maximum possible display resolution on the MIPI DSI interface of the i.MX6 [...] is 1280x720 pixels,

as specified in the Reference Manual document.

MIPI DSI max display resolution 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,266件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  "The maximum possible display resolution on the MIPI DSI interface of the i.MX6 [...] is 1280x720 pixels,

as specified in the Reference Manual document.

MIPI DSI max display resolution 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信