A problem about write external memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A problem about write external memory

1,353 Views
zhangzhiyong1
Contributor III

Hello ,I used IMX6Q in my design,There is a problem with me ,my design have a eMMC(8G Micron) and a uSSD(64G),I want test the memory.

step1  I use"dd if=/dev/zero of=/big_file bs=50M count=10",then It says"524288000 bytes (500.0MB) copied, 65.870651 seconds, 7.6MB/s",

step2 used"dd if=/dev/zero of=/big_file bs=50M count=10",then It says"524288000 bytes (500.0MB) copied, 98.181022 seconds, 5.1MB/s".

step3 hen I use "dd if=/dev/zero of=/big_file1 bs=50M count=10" then It says"

EXT3-fs error (device mmcblk0p1): ext3_free_blocks_sb: bit already cleared for block 6144
EXT3-fs error (device mmcblk0p1): ext3_free_blocks_sb: bit already cleared for block 6145
EXT3-fs error (device mmcblk0p1): ext3_free_blocks_sb: bit already cleared for block 6146
EXT3-fs error (device mmcblk0p1): ext3_free_blocks_sb: bit already cleared for block 6147

.......

"

and I can`t write  memory more than 600M.If I write more than 600M,the system breakdown。

what`s wrong ? what can I do ?

 

Labels (1)
0 Kudos
Reply
1 Reply

1,282 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhangzhiyong

this may be caused by overall board instability when writing much data

and reason can be ddr errors, ripples of power supplies, signal integrity issues.

Please refer to i.MX6 System Development User’s Guide to better identify source of problem.

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

ext3_free_blocks_sb: bit already cleared may mean ext3 error with
partition was mounted read-only again and flagged with an error code. Please check :
https://ubuntuforums.org/archive/index.php/t-1044387.html
https://bugzilla.redhat.com/show_bug.cgi?id=494927

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply