8bit data width LCDIF support in i.MX6SL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

8bit data width LCDIF support in i.MX6SL

跳至解决方案
1,598 次查看
ko-hey
Senior Contributor II

Hi all

I have a problem with the 8bit data width of LCDIF.

I'm trying to use LCDIF with 8bit data width in i.MX6SL.

Does the driver which is in NXP's BSP supports 8bit data width of LCDIF in i.MX6SL ?

According to the following thread, the driver doesn't support 8bit data width in i.MX6SX.

IMX6SX LCDIF 8bits 

In my understandings, the BSP use same driver in i.MX6 series.

Actually, the iMX6SL stuck when I tested with 8 bit data width.

On the other hand, it doesn't stick when I tested with other data width such as 16, 18, 24 bit

.Could you tell me whether the driver which is in NXP's BSP supports 8bit data width of LCDIF in i.MX6SL or not ?

Ko-hey

标签 (3)
标记 (3)
0 项奖励
回复
1 解答
1,362 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes, they are familar, refer to the Reference Manual, lcdif supports 8bit lcd, but in current bsp, which doesn't support it, just for 16,18 and 24

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,363 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes, they are familar, refer to the Reference Manual, lcdif supports 8bit lcd, but in current bsp, which doesn't support it, just for 16,18 and 24

0 项奖励
回复
1,362 次查看
ko-hey
Senior Contributor II

Hi Joan Xie

Thank you for reply.

Does NXP have any reference driver to support the 8bit lcd ?

Or do you know where to fix ?

Ko-hey

0 项奖励
回复
1,362 次查看
joanxie
NXP TechSupport
NXP TechSupport

I dont' find such driver for this, but if you use 8080 display on eLCDIF, maybe you can refer to this document, mx6 has the same LCDIF IP as mx50

https://community.nxp.com/thread/265022