8MMINILPD4-CPU2-DESIGNFILES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8MMINILPD4-CPU2-DESIGNFILES

Jump to solution
2,654 Views
Tori-san
Contributor III

Hello,

We are considering the SOM design with reference to 8MMINILPD4-CPU2.

The SPF-47712_A1.pdf file in 8MMINILPD4-CPU2-DESIGNFILES.zip contains the WIFI/BT Module(Page 10/13) and the SOM Interface(Page 13/13).

In addition, the explanation of "R116" in SOM Interface(Page 13/13) is as folows.

"When using M.2 WIFI Module on Base Board, remove R115, and populate R116!"

However, the WIFI/BT Module(Page 10/13) only has R215 resister as 32K CLKIN.

Isn't R115 described in the SOM Interface (page13/13) a typo in R215 ?

Best Regards,

Tori.

0 Kudos
Reply
1 Solution
2,628 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes,When using M.2 WIFI Module on Base Board, remove R215, and populate R116

View solution in original post

0 Kudos
Reply
3 Replies
2,639 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, you are right, for the new board use the R215, you can see it in the new schematic.

0 Kudos
Reply
2,633 Views
Tori-san
Contributor III

"When using M.2 WIFI Module on Base Board, remove R115, and populate R116!"

Above comment on "SOM Interface (page13/13)" shoule be replaced as follows, right?

"When using M.2 WIFI Module on Base Board, remove R215, and populate R116!"

Best Regards,

Tori.

2,629 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes,When using M.2 WIFI Module on Base Board, remove R215, and populate R116

0 Kudos
Reply