8MMINILPD4-CPU2-DESIGNFILES

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

8MMINILPD4-CPU2-DESIGNFILES

ソリューションへジャンプ
2,653件の閲覧回数
Tori-san
Contributor III

Hello,

We are considering the SOM design with reference to 8MMINILPD4-CPU2.

The SPF-47712_A1.pdf file in 8MMINILPD4-CPU2-DESIGNFILES.zip contains the WIFI/BT Module(Page 10/13) and the SOM Interface(Page 13/13).

In addition, the explanation of "R116" in SOM Interface(Page 13/13) is as folows.

"When using M.2 WIFI Module on Base Board, remove R115, and populate R116!"

However, the WIFI/BT Module(Page 10/13) only has R215 resister as 32K CLKIN.

Isn't R115 described in the SOM Interface (page13/13) a typo in R215 ?

Best Regards,

Tori.

0 件の賞賛
返信
1 解決策
2,627件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes,When using M.2 WIFI Module on Base Board, remove R215, and populate R116

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,638件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, you are right, for the new board use the R215, you can see it in the new schematic.

0 件の賞賛
返信
2,632件の閲覧回数
Tori-san
Contributor III

"When using M.2 WIFI Module on Base Board, remove R115, and populate R116!"

Above comment on "SOM Interface (page13/13)" shoule be replaced as follows, right?

"When using M.2 WIFI Module on Base Board, remove R215, and populate R116!"

Best Regards,

Tori.

2,628件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes,When using M.2 WIFI Module on Base Board, remove R215, and populate R116

0 件の賞賛
返信