8MHz clock generate out using PLL in i.mx6ull maximum possibilities pins in processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

8MHz clock generate out using PLL in i.mx6ull maximum possibilities pins in processor

1,204 次查看
prabhu1
Contributor III

Hi Igorpadykov,

Other than CCM_CLKO1,2 any other PLL pin possibilities to generate 8MHz clock out.

pastedImage_1.png

In above image CCM_CLKO1,2 are connected JTAG pins(JTAG_TMS and JTAG_TDO) Since JTAG  pins N15 or P14 has been used for 8MHZ clock, will that be conflicting when we use JTAG. So any other pins for 8MHz clock generate.

0 项奖励
回复
3 回复数

1,164 次查看
prabhu1
Contributor III

But I didn't see any clock divider option on a sec.18.7.18 for 8MHz

0 项奖励
回复

1,164 次查看
igorpadykov
NXP Employee
NXP Employee

one can try to output AUDIO_PLL (reprogram it to necessary frequency

using CCM_ANALOG_PLL_AUDIOn register) and dividers in AUDIO_DIV_LSB(MSB)

CCM_ANALOG_MISC2n.

Best regards
igor

0 项奖励
回复

1,164 次查看
igorpadykov
NXP Employee
NXP Employee

Hi prabhu

as another alternative one can consider LVDSCLK1 (CCM_CLK1_N, CCM_CLK1_P balls)

described in sect.18.7.18 Miscellaneous Register 1 (CCM_ANALOG_MISC1n) i.MX6ULL Reference Manual 

https://www.nxp.com/webapp/Download?colCode=IMX6ULLRM 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复