5 UART Channels

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

5 UART Channels

1,296件の閲覧回数
CircuitPeon
Contributor I

Hello,

 

I am using the IMX 8 QM and am having trouble finding information on the UARTs. I have used the two flow control UARTs (RS422 to UART Receiver)  and am wondering where to connect my next two.

Are the M40 GPIO/I2C and M42 GPIO/I2C able to be used as UART?

If not, where should I connect my RS232 to UART Transceiver?

 

Thank you!

ラベル(1)
0 件の賞賛
返信
1 返信

1,289件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Brandon

 

information about available uarts and muxing options can be found in

i.MX8QM Reference Manual, in particular Chapter 2 Memory Map.

Unfortunately currently it is not available on public web site, but can be obtained

through local marketing channels.

 

Best regards
igor

0 件の賞賛
返信