5 UART Channels

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

5 UART Channels

1,292 次查看
CircuitPeon
Contributor I

Hello,

 

I am using the IMX 8 QM and am having trouble finding information on the UARTs. I have used the two flow control UARTs (RS422 to UART Receiver)  and am wondering where to connect my next two.

Are the M40 GPIO/I2C and M42 GPIO/I2C able to be used as UART?

If not, where should I connect my RS232 to UART Transceiver?

 

Thank you!

0 项奖励
回复
1 回复

1,285 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Brandon

 

information about available uarts and muxing options can be found in

i.MX8QM Reference Manual, in particular Chapter 2 Memory Map.

Unfortunately currently it is not available on public web site, but can be obtained

through local marketing channels.

 

Best regards
igor

0 项奖励
回复