3V coin cell backup for imx93

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

3V coin cell backup for imx93

跳至解决方案
940 次查看
Gorka_3
Contributor II

Hello everyone,

I would like to know if there is any way to use a 3V Coin Cell battery backup for the NVCC_BBSM_1P8 power rail of the imx93 with the PCA9451A PMIC. As I must keep the RTC and Tampers working once the main supply has been shutted down, a Coin Cell backup is needed.

In the "4.1.3 Power architecture" section of the imx93 datasheet there is an image which shows the basic diagram for a backup battery.

Gorka_3_0-1726488269512.png

 

I wonder if there is a way to connect the 3V CC to the PMIC. In order to achive an uninterrumpted NVCC_BBSM_1P8 (provided by LDO1), I must keep INL1 and VSYS above 2.7V  due to the UVLO feature of the PMIC (which is impossible with a 3V CC). Anyway, a LDO with a CC would be pretty bad in terms of efficiency.

Is there any way to use a 3V CC backup alongside the PCA9451A to keep NVCC_BBSM_1P8 power rail on?

If no, is a power mux with ideal diodes needed to do a custom switchover between the PMIC's LDO output and a regulated (with a buck converter) 3V coin cell to manage this issue?

Best regards,

Gorka.

0 项奖励
回复
1 解答
917 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

As is mentioned in PMIC's datasheet, the suggested option is connect a battery and a regulator in NVCC_BBSM_1P8 power rail to keep this power domain on and switch between the PMIC's LDO and regulated output from coin cell.

Best regards.

在原帖中查看解决方案

0 项奖励
回复
1 回复
918 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

As is mentioned in PMIC's datasheet, the suggested option is connect a battery and a regulator in NVCC_BBSM_1P8 power rail to keep this power domain on and switch between the PMIC's LDO and regulated output from coin cell.

Best regards.

0 项奖励
回复