ADAU7002 device configuration not working - IMX8ULP-EVK9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADAU7002 device configuration not working - IMX8ULP-EVK9

852件の閲覧回数
dhruvinrajpura
Contributor III

I am attempting to connect a microphone to the A core of the IMX8ULP-EVK9 using the ADAU7002 IC. I've added the ADAU7002 node to my DTS file, but I'm encountering the following error.

[ 21.860836] platform sound-adau7002: deferred probe pending

 

I also checked this node with sai5 as well.

Can anyone check on this?...

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 返信

818件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

The ADAU7002 is not supported by default on our BSP. To use this converter in your system, maybe you need to add a third-party driver.

Unfortunately, there is not a guide to port this specific device to the BSP. The references we have are the i.MX porting guide and EVK device tree (WM8960).

Maybe these links could be helpful:

sound/soc/codecs/adau7002.c

Documentation/devicetree/bindings/sound/adi,adau7002.yaml

Best regards.

0 件の賞賛
返信