3LCD implementability by i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

3LCD implementability by i.MX6

ソリューションへジャンプ
6,495件の閲覧回数
george
Senior Contributor II

Dear all,

We have planned the Signage product for the amusements using i.MX6.

It has 3LCD panel.

It handles the unusual size image.

I want to know whether this can be implemented only by i.MX6.

pastedImage_0.png

For example, (1)HDMI, (2)LVDS, and (3)LVDS are available as a LCD interface.

Because it is Signage equipment, needed functions are pictures display and movie playback.

In others:

  • display these two in layers.
  • scan frequency is 15-30fps.

Is implementation possible?

When using BSP as the base, is many change needed for S/W?

Best Regards,

George

ラベル(4)
0 件の賞賛
返信
1 解決策
6,097件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

yes I think i.MX6QD can do that.

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
6,097件の閲覧回数
raimundszabo
Contributor II

Hi,

Have a look here. It might be useful: Re: Spanning GUI over multiple framebuffers

Regards,

Raimund

0 件の賞賛
返信
6,097件の閲覧回数
george
Senior Contributor II

Dear Raimond,

I will refer to it.

Thanks,

George

0 件の賞賛
返信
6,097件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

what is processor - Q, D, S, DL, SL  ?

Best regards

igor

0 件の賞賛
返信
6,097件の閲覧回数
george
Senior Contributor II

Dear Igor,

Thank you for the quick action.

The low cost possible product is desirable.

However, implementation of a function is the most important.

BR,

George

0 件の賞賛
返信
6,097件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

I think this is feasible only with i.MX6QD, since it

has 2xIPU. In my opinion sw changes may be significant,

also attached i.MX6QD porting guide.

MX6DQ_IPU.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

6,097件の閲覧回数
george
Senior Contributor II

Dear Igor,

I was glad that your opinion could be heard.

I think S/W change a few more after this.

Please let me know one.

Can multiple monitors be handled as one monitor virtually in such environment?

BR,

George

0 件の賞賛
返信
6,098件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

yes I think i.MX6QD can do that.

Best regards

igor

0 件の賞賛
返信
6,097件の閲覧回数
george
Senior Contributor II

Igor,

Thanks.

0 件の賞賛
返信