3LCD implementability by i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

3LCD implementability by i.MX6

跳至解决方案
6,549 次查看
george
Senior Contributor II

Dear all,

We have planned the Signage product for the amusements using i.MX6.

It has 3LCD panel.

It handles the unusual size image.

I want to know whether this can be implemented only by i.MX6.

pastedImage_0.png

For example, (1)HDMI, (2)LVDS, and (3)LVDS are available as a LCD interface.

Because it is Signage equipment, needed functions are pictures display and movie playback.

In others:

  • display these two in layers.
  • scan frequency is 15-30fps.

Is implementation possible?

When using BSP as the base, is many change needed for S/W?

Best Regards,

George

标签 (4)
标记 (5)
0 项奖励
回复
1 解答
6,151 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

yes I think i.MX6QD can do that.

Best regards

igor

在原帖中查看解决方案

0 项奖励
回复
8 回复数
6,151 次查看
raimundszabo
Contributor II

Hi,

Have a look here. It might be useful: Re: Spanning GUI over multiple framebuffers

Regards,

Raimund

0 项奖励
回复
6,151 次查看
george
Senior Contributor II

Dear Raimond,

I will refer to it.

Thanks,

George

0 项奖励
回复
6,151 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

what is processor - Q, D, S, DL, SL  ?

Best regards

igor

0 项奖励
回复
6,151 次查看
george
Senior Contributor II

Dear Igor,

Thank you for the quick action.

The low cost possible product is desirable.

However, implementation of a function is the most important.

BR,

George

0 项奖励
回复
6,151 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

I think this is feasible only with i.MX6QD, since it

has 2xIPU. In my opinion sw changes may be significant,

also attached i.MX6QD porting guide.

MX6DQ_IPU.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

6,151 次查看
george
Senior Contributor II

Dear Igor,

I was glad that your opinion could be heard.

I think S/W change a few more after this.

Please let me know one.

Can multiple monitors be handled as one monitor virtually in such environment?

BR,

George

0 项奖励
回复
6,152 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

yes I think i.MX6QD can do that.

Best regards

igor

0 项奖励
回复
6,151 次查看
george
Senior Contributor II

Igor,

Thanks.

0 项奖励
回复