3G modem on imx6 platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

3G modem on imx6 platform

ソリューションへジャンプ
5,711件の閲覧回数
javierw
Contributor II

Hello.


We have tried to add the 3G modem to our board, but failed.


Our board detail is as below:

Hardware:  imx6dq

OS:        Android 4.2.2 sabresd

3G modem:  Huawei MU609

3G modem interface: Mini PCIe


Is there any proposal on the design with 3G modem? 
W
hat 3G module the Freescale Android 4.2.2 BSP has supported successfully?


Thank you and hope that we can get some help from you.

1 解決策
4,016件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,017件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
4,014件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Javier

please look at p.3 attached Release Notes,

EM770W was tested,  however firmware may

be changed from time to time. So it may be recommended to check for

driver suitable for particular radio chip revision.

android-imx6-kitkat/0037-ENGR00281121-3G-Searching-Mobile-network-error-for-S.patch at master · rabe...

For ZTE FM210 modem there is a common option usb driver .

Kernel/drivers/usb/serial/option.c

May be helpful below link for Android PCIe WiFi

https://community.freescale.com/docs/DOC-94045

Best regards

igor

0 件の賞賛
返信
4,014件の閲覧回数
EricsEah
Contributor I


Can you help me to check which radio chip revision of EM770W is suitable for the driver of Android 4.2.2?  Thanks.

0 件の賞賛
返信