Deserializer in

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,725件の閲覧回数
takashitakahash
Contributor III

When capturing iMX6D RGB565 format via the deserializer In

What is the signal assignment of the data bus.

Which corresponding bits to each bit of  data bus  to  R [5:00], G [5:01], b [5:00] ?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,645件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,646件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
1,646件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

MIPI-CSI data bit placement is given in

sect.40.5.1 General/Arbitrary Data Reception

IMX6DQRM

as for CSI bit allocation one can look at

sect.4.11.10.1 IPU Sensor Interface Signal Mapping

IMX6DQCEC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信