3.10.31 GA release

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

3.10.31 GA release

Jump to solution
3,745 Views
huangxiongwei
Contributor I

Hello all

We are starting from a new project based on imx6

And I notice your linux based bsp final release is 3.10.31 beta

Do you have plan to release 3.10.31 GA version ?

Thanks and regards

Xiongwei

Labels (5)
0 Kudos
Reply
1 Solution
2,523 Views
SergioSolis
NXP Employee
NXP Employee

Yes, there are plans to release a GA version, though I'm not sure about the date yet.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,524 Views
SergioSolis
NXP Employee
NXP Employee

Yes, there are plans to release a GA version, though I'm not sure about the date yet.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,523 Views
huangxiongwei
Contributor I

Thanks

0 Kudos
Reply
2,523 Views
leige-b42127
Senior Contributor II

hi,黄雄伟,我是葛磊,以前在哈曼待过半年,离开哈曼后我来了飞思卡尔,有空常联系。

0 Kudos
Reply