Dear sir,
We have observed a 20% increase in power consumption during idle mode when comparing Yocto 4.0 (kernel 5.15.71-2.2.2) to Yocto 5.0 (kernel 6.6.52-2.2.0) on the NXP i.MX 8M Plus EVK.
Specifically, the measured power consumption during idle mode is as follows:
| | Yocto 4.0(kernel 5.15.71-2.2.2) | Yocto 5.0(kernel 5.15.71-2.2.2) |
Idle, Power consumption (measured on power-supply) | 5V, 413 mA | 5V, 510 mA |
Both tests were conducted using the prebuilt images downloaded from the NXP official website without any modifications:
- LF_v5.15.71-2.2.2_images_IMX8MPEVK.zip
- LF_v6.6.52-2.2.0_images_IMX8MPEVK.zip
This increase in power consumption might lead to a temperature difference of approximately 6-7 degrees Celsius on our custom board.
We have noted that the CPU usage and frequency remain similar between the two versions.
Could you please assist us in identifying the cause of this power consumption difference? Your insights would be greatly appreciated.
BR,
Richard