2 questions about mx31's CSI interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2 questions about mx31's CSI interface

4,483 次查看
Ken_Lin
Contributor I
Hi,everybody.
I'm new for the MX31.In my project, i must use MX31's Camera Sensor Interface. And my sensor output in BT.656 YUV422. But i have 2 questions about the CSI.
 
1. My sensor output 8-bits data, should i connect them to Mx31's CSI_D6~13 pins or CSI_D8~D15 pins or others?
2. How should I set the CSI CCIR Code Registers?
 
Should any one help me? Thanks.
0 项奖励
回复
5 回复数

2,599 次查看
Ken_Lin
Contributor I

Hi,DurianBoy

I found that Interlace 2 Progressive is a terrible job in MX31, and I've give up that idea.

I only use one field in 2 fields of a frame as many guys do.

It's a late reply, and i wish you've solved it.

0 项奖励
回复

2,599 次查看
enricobe
Contributor II
Hi, Ken,
by the way, does your camera send interlaced or progressive frame?
I've got values for CCIR registers with interlaced mode, but conversion from interlaced to progressive is not functional.

        __raw_writel(0x40596, CSI_CCIR_CODE_1);
        __raw_writel(0xD07DF, CSI_CCIR_CODE_2);
        __raw_writel(0xFF0000, CSI_CCIR_CODE_3);

E

0 项奖励
回复

2,599 次查看
DurianBoy
Contributor I

Hi Eric and Ken, I am also using an interlaced camera device and I need the MX35 to convert it to progressive mode before sending the buffer on to a computer VGA monitor. Did you guys get this to work?

What registers need to change to do this conversion?

 

Thanks a million!

0 项奖励
回复

2,599 次查看
enricobe
Contributor II
Hi,
you have to use D8-15 when using a 8-bit sensor/decoder.
Regards,
Enrico

0 项奖励
回复

2,599 次查看
ADUBOST
Contributor I
Hi,

I don't know if it will be usefull for you but I changed the original iMAGIC CMOS sensor by a video decoder on an iMX27 and i connected it on CSI D0-D7.

Bye

adubost
0 项奖励
回复