138 1 230-77452 Y1, 139 1 230-78102 Y2. These are the AgilePN shown on the MIMXRT1050-EVK BOM. Can you give me what the manufacturer's part number?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

138 1 230-77452 Y1, 139 1 230-78102 Y2. These are the AgilePN shown on the MIMXRT1050-EVK BOM. Can you give me what the manufacturer's part number?

2,084件の閲覧回数
williambyrd
Contributor I

Looking for the Manufacturer's part number for the oscillators on the MIMXRT1050-EVK schematic.

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,955件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello William Byrd,

There crystals used are:

XTAL 24MHZ -- 30PPM 3.2X2.5MM SMD for example: TXC 7V24000002

XTAL 32.768KHZ 7PF 20PPM – SMT for example: Epson Q13FC13500002

But you may use other PN if they adhere to the specifications.

Regards,

0 件の賞賛
返信

1,954件の閲覧回数
williambyrd
Contributor I

Thank you.

Bill

0 件の賞賛
返信