138 1 230-77452 Y1, 139 1 230-78102 Y2. These are the AgilePN shown on the MIMXRT1050-EVK BOM. Can you give me what the manufacturer's part number?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

138 1 230-77452 Y1, 139 1 230-78102 Y2. These are the AgilePN shown on the MIMXRT1050-EVK BOM. Can you give me what the manufacturer's part number?

2,090 Views
williambyrd
Contributor I

Looking for the Manufacturer's part number for the oscillators on the MIMXRT1050-EVK schematic.

Labels (3)
0 Kudos
Reply
2 Replies

1,961 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello William Byrd,

There crystals used are:

XTAL 24MHZ -- 30PPM 3.2X2.5MM SMD for example: TXC 7V24000002

XTAL 32.768KHZ 7PF 20PPM – SMT for example: Epson Q13FC13500002

But you may use other PN if they adhere to the specifications.

Regards,

0 Kudos
Reply

1,960 Views
williambyrd
Contributor I

Thank you.

Bill

0 Kudos
Reply