如何让bitbake采用git仓库相对路径下载代码?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

如何让bitbake采用git仓库相对路径下载代码?

2,833 Views
zbunix
Contributor I
如何让bitbake采用git仓库相对路径下载代码?

使用bitbake下载代码失败出错?
由于使用本地服务器采用git+gitolite管理代码,
只能采用git仓库相对路径(git@192.168.101.1:testing.git;protocol=ssh下载代码,不能采用绝对路径下载代码(git://git@192.168.101.1/home/git/repo/testing.git;;protocol=ssh

testing.git不使用bitake方式时候可以正常下载代码
---------------------------------------------------
```
$ git clone git@192.168.101.1:testing.git -b master
正克隆到 'testing'...
remote: Counting objects: 21, done.
remote: Compressing objects: 100% (16/16), done.
remote: Total 21 (delta 5), reused 0 (delta 0)
接收对象中: 100% (21/21), 320.39 KiB | 0 bytes/s, done.
处理 delta 中: 100% (5/5), done.
检查连接... 完成。
```

testing/testing.bb
-------------------------
```
DESCRIPTION = "testing"
LICENSE = "GPLv2+"
LIC_FILES_CHKSUM = "file://Licenses/gpl-2.0.txt;md5=b234ee4d69f5fce4486a80fdaf4a4263"
SRC_URI = "git://git@192.168.101.1:testing.git;protocol=ssh;branch=master"
SRCREV = "3d361c8b81cf783e4af8b1be6e7ada7bf9b9ef07"
S = "${WORKDIR}/git"
```

使用bitbake下载代码失败出错log
----------------------------------
```
$ bitbake -c fetch testing -v -f
Loading cache: 100% |##############################################################################################################################################################################| ETA:  00:00:00
Loaded 2631 entries from dependency cache.
Parsing recipes: 100% |############################################################################################################################################################################| Time: 00:00:00
Parsing of 2102 .bb files complete (2101 cached, 1 parsed). 2625 targets, 339 skipped, 4 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
NOTE: selecting pseudo-native to satisfy virtual/fakeroot-native due to PREFERRED_PROVIDERS
NOTE: selecting gcc-cross-arm to satisfy virtual/arm-poky-linux-gnueabi-gcc due to PREFERRED_PROVIDERS
NOTE: selecting gcc-runtime to satisfy virtual/arm-poky-linux-gnueabi-compilerlibs due to PREFERRED_PROVIDERS
NOTE: selecting glibc to satisfy virtual/libc due to PREFERRED_PROVIDERS
NOTE: selecting glibc to satisfy runtime libsegfault due to PREFERRED_PROVIDER_virtual/libc = glibc
NOTE: selecting glibc to satisfy runtime glibc-dev due to PREFERRED_PROVIDER_virtual/libc = glibc
NOTE: selecting glibc to satisfy runtime glibc due to PREFERRED_PROVIDER_virtual/libc = glibc
NOTE: selecting binutils-cross-arm to satisfy virtual/arm-poky-linux-gnueabi-binutils due to PREFERRED_PROVIDERS
NOTE: selecting glibc to satisfy virtual/arm-poky-linux-gnueabi-libc-for-gcc due to PREFERRED_PROVIDERS
NOTE: selecting linux-libc-headers to satisfy linux-libc-headers due to PREFERRED_PROVIDERS
NOTE: selecting gcc-cross-arm to satisfy virtual/arm-poky-linux-gnueabi-g++ due to PREFERRED_PROVIDERS
NOTE: selecting libgcc to satisfy libgcc due to PREFERRED_PROVIDERS
NOTE: selecting gcc-cross-initial-arm to satisfy virtual/arm-poky-linux-gnueabi-gcc-initial due to PREFERRED_PROVIDERS
NOTE: selecting glibc-initial to satisfy virtual/arm-poky-linux-gnueabi-libc-initial due to PREFERRED_PROVIDERS
NOTE: selecting linux-libc-headers to satisfy runtime linux-libc-headers-dev due to PREFERRED_PROVIDER_linux-libc-headers = linux-libc-headers
NOTE: selecting libgcc to satisfy runtime libgcc due to PREFERRED_PROVIDER_libgcc = libgcc

Build Configuration:
BB_VERSION        = "1.26.0"
BUILD_SYS         = "x86_64-linux"
NATIVELSBSTRING   = "Ubuntu-14.04"
TARGET_SYS        = "arm-poky-linux-gnueabi"
MACHINE           = "imx6qsabresd"
DISTRO            = "fsl-imx-fb"
DISTRO_VERSION    = "3.14.52-1.1.0"
TUNE_FEATURES     = "arm armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU        = "vfp-neon"
meta              
meta-yocto        = "(nobranch):b74ea963cefffad9fbd91d4eb9b240f6a8c86cd0"
meta-oe           
meta-multimedia   = "(nobranch):df2f700d66bace65f5d802225232d01cf511fe81"
meta-fsl-arm      = "(nobranch):70ddee3ebeacbc53180ee7221533375bf0c9eac4"
meta-fsl-arm-extra = "(nobranch):41e79c6bd055f12b6252618c22c43a2fed5cfb49"
meta-fsl-demos    = "(nobranch):17f9da65efb5c65c1d44b5cc18584034b29a742b"
meta-bsp          
meta-sdk          = "(nobranch):6a96fe97d411e097d2222c8e93198b558f4c0329"
meta-browser      = "(nobranch):30b8d6b3d0d6501c56ef6967a2fa73a3d4bf5fe9"
meta-gnome        
meta-networking   
meta-python       
meta-ruby         
meta-filesystems  = "(nobranch):df2f700d66bace65f5d802225232d01cf511fe81"
meta-itas-demo    = "<unknown>:<unknown>"
meta-qt5          = "(nobranch):51b4620392aa9041d8512549bfa554bea368c5ea"

NOTE: Preparing RunQueue
NOTE: Marking Active Tasks
NOTE: Pruned 1296 inactive tasks, 1 left
NOTE: Assign Weightings
NOTE: Compute totals (have 1 endpoint(s))
NOTE: Invalidate task do_fetch, /home/test/fsl-releases-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/testing/testing.bb
NOTE: Tainting hash to force rebuild of task /home/test/fsl-releases-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/testing/testing.bb, do_fetch
WARNING: /home/test/fsl-releases-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/testing/testing.bb.do_fetch is tainted from a forced run
NOTE: Executing RunQueue Tasks
WARNING: Failed to fetch URL git://git@192.168.101.1:testing.git;protocol=ssh;branch=master, attempting MIRRORS if available
ERROR: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/home/test/fsl-releases-bsp/downloads//git2/192.168.101.91:testing.git'...
fatal: No path specified. See 'man git-pull' for valid url syntax

ERROR: Function failed: Fetcher failure for URL: 'git://git@192.168.101.1:testing.git;protocol=ssh;branch=master'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/test/fsl-releases-bsp/fsl-imx-fb/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/testing/1.0-r0/temp/log.do_fetch.20491
ERROR: Task 0 (/home/test/fsl-releases-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/testing/testing.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1 tasks of which 0 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
  /home/test/fsl-releases-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/testing/testing.bb, do_fetch
Summary: There were 2 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
```
Labels (1)
0 Kudos
Reply
1 Reply

2,243 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

Please verify that you have internet connection and you may contact your system administrator because if you are using firewalls or proxy server this may avoid connection.

 

Besides, for one or the other reason the GIT server is sometimes not reachable, but you still have the option to download the source code from Freescale Public GIT  (http://git.freescale.com/git/) and then build it. If you have the need for various builds based on the same release, then it's useful to download all sources one time and base the following builds then on (a copy of) the local sources:

 

$ bitbake -c fetchall target


In Yocto Project Development Manual (http://www.yoctoproject.org/docs/2.0/dev-manual/dev-manual.html) in chapter 5.15 you find some more information.

Regards

0 Kudos
Reply