关于使用yocto工程编译内核的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于使用yocto工程编译内核的问题

Jump to solution
3,778 Views
jingyangxie
Contributor V

我按照《Freescale_Yocto_Project_User's_Guide.pdf》文档,搭建编译环境,并使用bitbake fsl-image-qt5命令,执行完成后,没有找到内核源代码(我用的bsp包是imx-4.1.15-1.2.0),请问

1、这个内核源代码在yocto工程里面是怎么分布的?

2、如果内核编译成功,fsl-image-qt5对应的文件系统是否含有QT5应用程序所需求的依赖库?

3、如何在PC端使用yocto开发QT应用程序,并交叉编译成IMX 6Solo X 所能支持的版本?

Labels (3)
0 Kudos
Reply
1 Solution
1,670 Views
jimmychan
NXP TechSupport
NXP TechSupport

the linux source code is located in the <build folder>/tmp/work/<board name>-poky-linux-gnueabi/linux-imx/

this link may useful for you. Setting up Qt Creator to build for i.MX6

View solution in original post

2 Replies
1,671 Views
jimmychan
NXP TechSupport
NXP TechSupport

the linux source code is located in the <build folder>/tmp/work/<board name>-poky-linux-gnueabi/linux-imx/

this link may useful for you. Setting up Qt Creator to build for i.MX6

1,670 Views
jingyangxie
Contributor V

自己先MARK一下

0 Kudos
Reply