Imx6 output file descriptions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx6 output file descriptions

992 次查看
santhosha
Contributor II

After finishing bitbake,  I can see these many images under /tmp/deploy/images folder.  Please describe what each of these images does.   Also let me know which of them need to be used for flashing in imx target board.

core-image-minimal-imx6qsabresd-20160629055409.rootfs.ext3
core-image-minimal-imx6qsabresd-20160629055409.rootfs.manifest
core-image-minimal-imx6qsabresd-20160629055409.rootfs.sdcard
core-image-minimal-imx6qsabresd-20160629055409.rootfs.tar.bz2
core-image-minimal-imx6qsabresd.ext3 -> core-image-minimal-imx6qsabresd-20160629055409.rootfs.ext3
core-image-minimal-imx6qsabresd.manifest -> core-image-minimal-imx6qsabresd-20160629055409.rootfs.manifest
core-image-minimal-imx6qsabresd.sdcard -> core-image-minimal-imx6qsabresd-20160629055409.rootfs.sdcard
core-image-minimal-imx6qsabresd.tar.bz2 -> core-image-minimal-imx6qsabresd-20160629055409.rootfs.tar.bz2
modules--3.10.17-r0-imx6qsabresd-20160629055409.tgz
modules-imx6qsabresd.tgz -> modules--3.10.17-r0-imx6qsabresd-20160629055409.tgz
README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt
u-boot.imx -> u-boot-imx6qsabresd-v2014.01-r0.imx
u-boot-imx6qsabresd.imx -> u-boot-imx6qsabresd-v2014.01-r0.imx
u-boot-imx6qsabresd-v2014.01-r0.imx
uImage -> uImage--3.10.17-r0-imx6qsabresd-20160629055409.bin
uImage--3.10.17-r0-imx6qsabresd-20160629055409.bin
uImage--3.10.17-r0-imx6q-sabresd-20160629055409.dtb
uImage--3.10.17-r0-imx6q-sabresd-hdcp-20160629055409.dtb
uImage--3.10.17-r0-imx6q-sabresd-ldo-20160629055409.dtb
uImage-imx6qsabresd.bin -> uImage--3.10.17-r0-imx6qsabresd-20160629055409.bin
uImage-imx6q-sabresd.dtb -> uImage--3.10.17-r0-imx6q-sabresd-20160629055409.dtb
uImage-imx6q-sabresd-hdcp.dtb -> uImage--3.10.17-r0-imx6q-sabresd-hdcp-20160629055409.dtb
uImage-imx6q-sabresd-ldo.dtb -> uImage--3.10.17-r0-imx6q-sabresd-ldo-20160629055409.dtb

-rw-r--r-- 1 santhosh santhosh 67108864 Jun 29 12:03 core-image-minimal-imx6qsabresd-20160629055409.rootfs.ext3
-rw-r--r-- 1 santhosh santhosh      978 Jun 29 12:03 core-image-minimal-imx6qsabresd-20160629055409.rootfs.manifest
-rw-r--r-- 1 santhosh santhosh 83886080 Jun 29 12:03 core-image-minimal-imx6qsabresd-20160629055409.rootfs.sdcard
-rw-r--r-- 1 santhosh santhosh  2285152 Jun 29 12:03 core-image-minimal-imx6qsabresd-20160629055409.rootfs.tar.bz2
lrwxrwxrwx 1 santhosh santhosh       58 Jun 29 12:03 core-image-minimal-imx6qsabresd.ext3 -> core-image-minimal-imx6qsabresd-20160629055409.rootfs.ext3
lrwxrwxrwx 1 santhosh santhosh       62 Jun 29 12:03 core-image-minimal-imx6qsabresd.manifest -> core-image-minimal-imx6qsabresd-20160629055409.rootfs.manifest
lrwxrwxrwx 1 santhosh santhosh       60 Jun 29 12:03 core-image-minimal-imx6qsabresd.sdcard -> core-image-minimal-imx6qsabresd-20160629055409.rootfs.sdcard
lrwxrwxrwx 1 santhosh santhosh       61 Jun 29 12:03 core-image-minimal-imx6qsabresd.tar.bz2 -> core-image-minimal-imx6qsabresd-20160629055409.rootfs.tar.bz2
-rw-rw-r-- 2 santhosh santhosh   599286 Jun 29 11:57 modules--3.10.17-r0-imx6qsabresd-20160629055409.tgz
lrwxrwxrwx 1 santhosh santhosh       51 Jun 29 11:57 modules-imx6qsabresd.tgz -> modules--3.10.17-r0-imx6qsabresd-20160629055409.tgz
-rw-r--r-- 2 santhosh santhosh      294 Jun 29 12:01 README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt
lrwxrwxrwx 1 santhosh santhosh       35 Jun 29 07:17 u-boot.imx -> u-boot-imx6qsabresd-v2014.01-r0.imx
lrwxrwxrwx 1 santhosh santhosh       35 Jun 29 07:17 u-boot-imx6qsabresd.imx -> u-boot-imx6qsabresd-v2014.01-r0.imx
-rwxr-xr-x 2 santhosh santhosh   314368 Jun 29 07:17 u-boot-imx6qsabresd-v2014.01-r0.imx
lrwxrwxrwx 1 santhosh santhosh       50 Jun 29 11:57 uImage -> uImage--3.10.17-r0-imx6qsabresd-20160629055409.bin
-rw-r--r-- 2 santhosh santhosh  5264672 Jun 29 11:57 uImage--3.10.17-r0-imx6qsabresd-20160629055409.bin
-rw-r--r-- 2 santhosh santhosh    47179 Jun 29 11:57 uImage--3.10.17-r0-imx6q-sabresd-20160629055409.dtb
-rw-r--r-- 2 santhosh santhosh    47268 Jun 29 11:57 uImage--3.10.17-r0-imx6q-sabresd-hdcp-20160629055409.dtb
-rw-r--r-- 2 santhosh santhosh    47179 Jun 29 11:57 uImage--3.10.17-r0-imx6q-sabresd-ldo-20160629055409.dtb
lrwxrwxrwx 1 santhosh santhosh       50 Jun 29 11:57 uImage-imx6qsabresd.bin -> uImage--3.10.17-r0-imx6qsabresd-20160629055409.bin
lrwxrwxrwx 1 santhosh santhosh       51 Jun 29 11:57 uImage-imx6q-sabresd.dtb -> uImage--3.10.17-r0-imx6q-sabresd-20160629055409.dtb
lrwxrwxrwx 1 santhosh santhosh       56 Jun 29 11:57 uImage-imx6q-sabresd-hdcp.dtb -> uImage--3.10.17-r0-imx6q-sabresd-hdcp-20160629055409.dtb
lrwxrwxrwx 1 santhosh santhosh       55 Jun 29 11:57 uImage-imx6q-sabresd-ldo.dtb -> uImage--3.10.17-r0-imx6q-sabresd-ldo-20160629055409.dtb

标签 (1)
0 项奖励
回复
1 回复

892 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Please download the BSP documentation from here:

i.MX 6 Series Software and Development Tool|NXP

Basically, all the information can be found from the Freescale_Yocto_Project_User's_Guide and i.MX_Linux_User's_Guide.

All the drivers information can be found in i.MX_Linux_Reference_Manual

0 项奖励
回复