i.mx8M EVK board encoder and decoder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx8M EVK board encoder and decoder

i.mx8M EVK board encoder and decoder

i.mx8M evk board has HW decoder and SW encoder, this document introduce how to use HW decoder and SW encoder

the bsp is the latest version L4.14.78, the environment is :

$ DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland

$ bitbake fsl-image-validation-imx

 

For the 4.14.78, we don’t use mfgtool anymore, customer can use uuu.exe to program the image to the board, the uuu.exe can be found from https://github.com/NXPmicro/mfgtools/releases

Here we use emmc as media, I attached the kerel_emmc.uuu for reference

Open the cmd.exe, then use the command “uuu.exe kernel_emmc.uuu” to download the image to the emmc on the board as the picture shows

pastedImage_9.png

When the board boot up, don’t forget to change the image and fdt_file as you want, for example, I use Image-imx8mqevk.bin as image name  and Image-fsl-imx8mq-evk.dtb as my fdt file, you can choose different image and fdt file as uuu file mentions.

pastedImage_10.png

1) Decoding

 

For play the video, we can use three solution to support this

a) gplay-1.0 test.mp4

b) gst-launch-1.0 playbin uri=file:///mnt/sdcard/test.mp4

c) gst-launch-1.0 filesrc location=test.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! autovideosink

For play the two different video to the different display, current imx8M evk board supports dual hdmi output, in the uboot command:

setenv fdt_file Image-fsl-imx8mq-evk-dual-display.dtb

saveenv

Use the command as below:

   gst-launch-1.0 playbin uri=file:///test1.mp4 playbin uri=file:///test2.mp4 video-sink="glimagesink display-master=false display-slave=true"

2) Encoding

Because imx8M evk don’t have hardware encoding, so we need to add the SW plugins in the bsp

  a)add the commands as below in the /build/conf/local.conf

"CORE_IMAGE-EXTRA_INSTALL += "gstreamer1.0-plugins-ugly-meta packagegroup-fsl-gsstreamer1.0-commercial gst-ffmpeg"

LICENSE_FLAGS_WHITELIST = "commercial""

       b)Create the new txt file and add “PACKAGECONFIG_mx8mq = "x264"”in the file

       c)Rename the file as 0-plugins-ugly_%.bbappend and put this file under /sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/gstreamer

       d)Build the image you want, then download the new rootfs file in the board, use the command “gst-inspect-1.0 | grep x264”

pastedImage_12.png

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎03-30-2019 03:07 AM
更新者: