i.MX6 USB Mass Storage Driver Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 USB Mass Storage Driver Problem

i.MX6 USB Mass Storage Driver Problem

Hi all,

     I have a problem about usb mass storage driver, that's it can't enumerate my mass storage device.

     but it can enumerate my mouse, keyboard...etc hid device.

     anyone have idea about it ?

     I always get below messages when my mass storage device plugs in.

IMAG0319.jpg

     and below is my dmesg information

IMAG0320.jpg

     My hardware -->

     Type A receptacle on otg controller ~

Labels (2)
Tags (2)
Comments

Hi, I'm having the same issue, investigating now.  Have you made any progress or have a solution?

I'm not using the OTG port, but I am getting similar messages.

Hi Ken,

My issue had been fixed…but I didn’t do anything, that’s HW issue.

Best regards,

Hi wangyc,

This was posted as a document, and not as a discussion. I think you are more likely to get a response if you re-post it as a discussion. You can do that by following this link:

https://community.freescale.com/community/post!input.jspa?containerType=14&container=2004&contentTyp...

Let me know if this helps.

Thanks,

Jodi Paul

Community Administrator

Hi,

Maybe the difference between mass storage and HID devices is the speed.

Is this a custom board? Then check the layout and routing of the USB differential data lines.

Also, do you supply the USB PHY of the i.MX6 properly?

Best regards,

Harald Krapfenbauer

Bluetechnix

No ratings
Version history
Last update:
‎04-17-2013 06:01 PM
Updated by: