i.MX U-boot Configuration for Display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX U-boot Configuration for Display

i.MX U-boot Configuration for Display

Since U-Boot can read/write/update nodes inside the device tree blob before booting the kernel, the idea is to have a generic display node in the device tree which U-Boot will populate with the proper values.

You can see in our source tree that all our device trees contain:

fb_hdmi alias to setup HDMI configuration

fb_lcd alias to setup LCD displays fb_lvds and t_lvds to setup LVDS1 display

fb_lvds2 and t_lvds2 to setup LVDS2 display (when available)

So U-Boot is now is charged to setup those nodes which will configure your display(s) easily.

First of all it requires the U-Boot, Once you have a recent U-Boot, you can have a look at the supported display for your board by issuing:

=> fbpanel clock-frequency hactive vactive hback-porch hfront-porch vback-porch vfront-porch hsync-len vsync-len hdmi: 1280x720M@60:m24x1,50:74161969,1280,720,220,110,20,5,40,5 74161969 1280 720 220 110 20 5 40 5 hdmi: 1920x1080M@60:m24x1,50:148500148,1920,1080,148,88,36,4,44,5 148500148 1920 1080 148 88 36 4 44 5 ...

Since the list is actually pretty long and not always easy to read, you can also filter by type of display (hdmi, lcd or lvds)

=> fbpanel lcd clock-frequency hactive vactive hback-porch hfront-porch vback-porch vfront-porch hsync-len vsync-len lcd: fusion7:m18x2,10:33264586,800,480,96,24,31,11,136,3 33264586 800 480 96 24 31 11 136 3 lcd: CLAA-WVGA:m18x2,48:27000027,800,480,40,60,10,10,20,10 27000027 800 480 40 60 10 10 20 10 ... => fbpanel lvds clock-frequency hactive vactive hback-porch hfront-porch vback-porch vfront-porch hsync-len vsync-len lvds: hannstar7:18x2,38:71108582,1280,800,80,48,15,2,32,6 71108582 1280 800 80 48 15 2 32 6 ...

The above command just lists the available displays, when you want to set one, you need will to set the following variables:

  • fb_hdmi controls HDMI display selection
  • fb_lcd controls LCD display selection
  • fb_lvds controls LVDS display selection
  • fb_lvds2 controls LVDS2 display selection

Also, when a display isn't used, you need to set it to off. Here is an example on how to setup the HDMI to display at 1080P and LVDS display to be the Hannstar 10'

=> setenv fb_lvds hannstar => setenv fb_hdmi 1920x1080M@60 => setenv fb_lcd off => saveenv Saving Environment to SPI Flash... SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB Erasing SPI flash...Writing to SPI flash...done => reset

Once rebooted, you can have a look at the cmd_hdmi, cmd_lcd and cmd_lvds that U-Boot will have set

=> print cmd_hdmi cmd_hdmi=fdt set fb_hdmi status okay;fdt set fb_hdmi mode_str 1920x1080M@60; => print cmd_lvds cmd_lvds=fdt set fb_lvds status okay;fdt set fb_lvds interface_pix_fmt RGB666;fdt set ldb/lvds-channel@0 fsl,data-width ;fdt set ldb/lvds-channel@0 fsl,data-mapping spwg;fdt set t_lvds clock-frequency ;fdt set t_lvds hactive ;fdt set t_lvds vactive ;fdt set t_lvds hback-porch ;fdt set t_lvds hfront-porch ;fdt set t_lvds vback-porch ;fdt set t_lvds vfront-porch ;fdt set t_lvds hsync-len ;fdt set t_lvds vsync-len ; => print cmd_lcd cmd_lcd=fdt set fb_lcd status disabled

Do not try to set those cmd_* variables yourself, they will be overwritten by U-Boot at bootup anyway.

That's it, you should now be able to list, select and setup the displays the way you want.

For another type of display, It depends on the type of display:

  • LVDS: yes, since all the timings are inside the device tree node you can change them.

Here is an example for our latest 7"1280x800 display, although only the latest U-Boot binary lists it, you can have it running by entering:

=> setenv fb_lvds tm070jdhg30:24:68152388,1280,800,5,63,2,39,1,1 => saveenv

Note that it goes like this:

setenv fb_xxx mode_str:connection-type:clk-frequency,hactive,vactive,hback-porch,hfront-porch,vback-porch,vfront-porch,hsync-len,vsync-len

The connection-type is very important since it allows to specify:

  • The data mapping: default is SPWG, need to add "j" to switch to JEIDA
  • The split mode: for dual LVDS channels operations (for 1080P display for instance) need to add "s"
  • The data width: can be 18 or 24

For instance, here is a fb_lvds setup for a dual channel JEIDA LVDS display with 24-bit witdth:

=> setenv fb_lvds 1080P60:js24:148500148,1920,1080,148,88,36,4,44,5

  • LCD: yes for U-Boot display, no for the kernel

You can set the fb_lcd like it is done for LVDS above, however the timings will only be used to setup U-Boot, only the mode_str will be passed on to the kernel. This means that the kernel needs to know about the LCD beforehand.

Here is an example for the ASIT500MA6F5D display:

=> setenv fb_lcd ASIT500MA6F5D:m24:32341861,800,480,88,40,32,13,48,3 => saveenv

  • HDMI: yes (well more or less)

Same as the LCD setting, only the mode_str is passed on to the kernel. The difference is that it can work out of the box on the kernel side if you ask for a standard resolution and standard refresh rate.

For instance, setting fb_hdmi to 1920x1080M@30 will work automatically since the kernel is smart enough to recognize a known resolution (1080P) with a standard refresh rate (30fps).

 

 

无评分
版本历史
最后更新:
‎10-09-2024 12:05 PM
更新人: