i.MX Development Miscellanea(i.MX 开发杂记)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Development Miscellanea(i.MX 开发杂记)

i.MX Development Miscellanea(i.MX 开发杂记)

  Just sharing some experiences during the development and studying.

  Although, it appears some hardwares, it focuses on software to speed up your developing on your  hardware.

 

  杂记共享一下在开发和学习过程中的经验。 

  虽然涉及一些硬件,但其本身关注软件,希望这些能加速您在自己硬件上的开发。

07/25/2024

iMX secondary boot collection
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-secondary-boot-collection/ta-p/19169...

 

07/25/2024

HSM Code-Signing Journey
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244

25JUL2024 - add pkcs11 proxy

                        HSM Code-Signing Journey_25JUL2024.pdf

                         HSM Code-Signing Journey_25JUL2024.txt

 

06/06/2024

HSM Code-Signing Journey
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/HSM-Code-Signing-Journey/ta-p/1882244

 

 

02/07/2024

Device Tree Standalone Compile under Windows
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Device-Tree-Standalone-Compile-under-Win...

 

02/07/2024

i.MX8X security overview and AHAB deep dive

i.MX8X security overview and AHAB deep dive - NXP Community

 

11/23/2023

“Standalone” Compile Device Tree

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Standalone-Compile-Device-Tree/ta-p/1762...

 

 

10/26/2023

Linux Dynamic Debug
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Linux-Dynamic-Debug/ta-p/1746611

 

08/10/2023

u-boot environment preset for sdcard mirror

u-boot environment preset for sdcard mirror - NXP Community

 

06/06/2023

all(bootloader, device tree, Linux kernel, rootfs) in spi nor demo imx8qxpc0 mek

all(bootloader, device tree, Linux kernel, rootfs)... - NXP Community

 

 

09/26/2022

parseIVT - a script to help i.MX6 Code Signing

parseIVT - a script to help i.MX6 Code Signing - NXP Community

 

Provide  run under windows

 

09/16/2022

 

create sdcard mirror under windows


create sdcard mirror under windows - NXP Community

 

 

08/03/2022

 

i.MX8MM SDCARD Secondary Boot Demo
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/...

 

 

02/16/2022


mx8_ddr_stress_test without UI

 

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/mx8-ddr-stress-test-without-UI/ta-p/1414...

 

12/23/2021


i.MX8 i.MX8X Board Reset
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-i-MX8X-Board-Reset/ta-p/1391130

 

 

 

12/21/2021


regulator userspace-consumer
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/regulator-userspace-consumer/ta-p/138994...

 

 

11/24/2021


crypto af_alg blackkey demo
crypto af_alg blackkey demo - NXP Community

 

09/28/2021


u-boot runtime modify Linux device tree(dtb)
u-boot runtime modify Linux device tree(dtb) - NXP Community

 

 

08/17/2021


gpio-poweroff demo
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/gpio-poweroff-demo/ta-p/1324306

 

 

 

 

08/04/2021


How to use gpio-hog demo
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709

 

 

 

07/14/2021


SWUpdate OTA i.MX8MM EVK / i.MX8QXP MEK
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta...

 

 

04/07/2021

i.MX8QXP eMMC Secondary Boot

https://community.nxp.com/t5/i-MX-Community-Articles/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45

 

 

 

03/25/2021

sc_misc_board_ioctl to access the M4 partition from A core side

sc_misc_board_ioctl to access the M4 partition fr... - NXP Community

 

 

03/17/2021

How to Changei.MX8X MEK+Base Board  Linux Debug UART

https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8X-MEK-Base-Board-Linux-Debug...

 

 

03/16/2021

How to Change i.MX8MM evk Linux Debug UART

https://community.nxp.com/t5/i-MX-Community-Articles/How-to-Change-i-MX8MM-evk-Linux-Debug-UART/ba-p...

 

 

 

05/06/2020

Linux fw_printenv fw_setenv to access U-Boot's environment variables

Linux fw_printenv fw_setenv to access U-Boot's env... - NXP Community

 

 

03/30/2020

i.MX6 DDR calibration/stress for Mass Production

https://community.nxp.com/docs/DOC-346065

 

 

03/25/2020

parseIVT - a script to help i.MX6 Code Signing
https://community.nxp.com/docs/DOC-345998

 

 

02/17/2020
Start your machine learning journey from tensorflow playground

Start your machine learning journey from tensorflow playground 

 

 

01/15/2020
How to add  iMX8QXP PAD(GPIO) Wakeup

How to add iMX8QXP PAD(GPIO) Wakeup 

 

01/09/2020
Understand iMX8QX Hardware Partitioning By Making M4 Hello world Running Correctly
https://community.nxp.com/docs/DOC-345359

 

09/29/2019

Docker On i.MX6UL With Ubuntu16.04

 

09/25/2019
Docker On i.MX8MM With Ubuntu
https://community.nxp.com/docs/DOC-344473
Docker On i.MX8QXP With Ubuntu
 

 

08/28/2019

eMMC5.0 vs eMMC5.1
https://community.nxp.com/docs/DOC-344265

 

 

05/24/2019

How to upgrade  Linux Kernel and dtb on eMMC without UUU

How to upgrade Linux Kernel and dtb on eMMC without UUU  

 

04/12/2019

eMMC RPMB Enhance and GP
https://community.nxp.com/docs/DOC-343116

 

04/04/2019

How to Dump a GPT SDCard Mirror(Android O SDCard Mirror)

https://community.nxp.com/docs/DOC-343079

 

04/04/2019

i.MX Create Android SDCard Mirror
https://community.nxp.com/docs/DOC-343078

 

04/02/2019:
i.MX Linux Binary_Demo Files Tips 
https://community.nxp.com/docs/DOC-343075

 

04/02/2019:
      Update Set fast boot 
      eMMC_RPMB_Enhance_and_GP.pdf

 

02/28/2019:

imx_builder --- standalone build without Yocto

https://community.nxp.com/docs/DOC-342702

 

08/10/2018:

i.MX6SX M4 MPU Settings For RPMSG update 

 

Update slide CMA Arrangement Consideration

i.MX6SX_M4_MPU_Settings_For_RPMSG_08102018.pdf

 

07/26/2018

Understand ML With Simplest Code

https://community.nxp.com/docs/DOC-341099

 

 

04/23/2018:

    i.MX8M Standalone Build

    i.MX8M Standalone Build.pdf

 

 

04/13/2018:

     i.MX6SX M4 MPU Settings For RPMSG  update
      

    Add slide CMA Arrangement  Consideration

    i.MX6SX_M4_MPU_Settings_For_RPMSG_04132018.pdf

 

09/05/2017:

      Update eMMC RPMB, Enhance  and GP

      eMMC_RPMB_Enhance_and_GP.pdf

09/01/2017:

      eMMC RPMB, Enhance  and GP

      eMMC_RPMB_Enhance_and_GP.pdf

08/30/2017:

    Dual LVDS for High Resolution Display(For i.MX6DQ/DLS)

    Dual LVDS for High Resolution Display.pdf

08/27/2017: 

  • L3.14.28 Ottbox Porting Notes:

        L3.14.28_Ottbox_Porting_Notes-20150805-2.pdf

  • MFGTool Uboot Share With the Normal Run One:

       MFGTool_Uboot_share_with_NormalRun_sourceCode.pdf

  • Mass Production with programmer

       Mass_Production_with_NAND_programmer.pdf

       Mass_Production_with_emmc_programmer.pdf

       L3.10.53_PianoPI_PortingNote_151102.pdf

  • Audio Codec WM8960 Porting L3.10.53 PianoPI

       AudioCodec_WM8960_Porting_L3.10.53_PianoPI_151012.pdf

  • TouchScreen PianoPI Porting Note

        TouchScreen_PianoPI_PortingNote_151103.pdf

  • Accessing GPIO From UserSpace

       Accessing_GPIO_From_UserSpace.pdf

       https://community.nxp.com/docs/DOC-343344

  • FreeRTOS for i.MX6SX

       FreeRTOS for i.MX6SX.pdf

  • i.MX6SX M4 fastup

       i.MX6SX M4 fastup.pdf

  • i.MX6 SDCARD Secondary Boot Demo

       i.MX6_SDCARD_Secondary_Boot_Demo.pdf

  • i.MX6SX M4 MPU Settings For RPMSG

       i.MX6SX_M4_MPU_Settings_For_RPMSG_10082016.pdf

  • Security

       Security03172017.pdf    NOT related to i.MX, only a short memo

コメント

Hi Biyong,

     Your documents are always helpful, thank you for sharing! I checked the latest "Generate Blob Under Linux" document, but it seems the link doesn't work. Can you please check the link again? Thank you!

Best Regards,

Frank

I don't know about what happened.

I use another way to  populate the document.

You can check it can link you to the right place.

And Please let me know it works or not. 

Hi Biyong,

    It works! Thank you and look forward for your new document.

Best Regards,

Frank

Cool! They are so useful.

Thank you for your sharing!

Looking forward to your update :)

100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎07-25-2024 12:07 AM
更新者: