Recently I published this i.MX Dev Blog post about the Gateworks plugin gst-variable-rtsp-server support for i.MX 6.
Now, you can check how to use it on i.MX 8 SoCs as well.
1. Preparing the image
In order to use gst-variable-rtsp-server plugin, prepare your machine and distro:
Add the following line to conf/local.conf:
IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server gst-variable-rtsp-server"Download the attached patch and apply it by doing:
$ cd <yocto_path>/sources/meta-fsl-bsp-release/ $ git am ~/Download/0001-Add-RTSP-support-for-i.MX-8-L4.14.78_ga1.0.0-or-olde.patch
Note: This patch is not necessary for L4.14.98_ga2.0.0 BSP!
Then, build the image with bitbake and deploy it to the SD card.
2. Video Test Source Example
Server
$ gst-variable-rtsp-server -p 9001 -u "videotestsrc ! v4l2h264enc ! rtph264pay name=pay0 pt=96"
Client
2. Camera Example
Server
$ gst-variable-rtsp-server -p 9001 -u "v4l2src device=/dev/video0 ! video/x-raw,width=640,height=480 ! v4l2h264enc ! rtph264pay name=pay0 pt=96"
Client
In order to use VLC or other application as the client, just enter the URL as shown in the image below:
IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server gst-variable-rtsp-server"Correct me if I am wrong but one will also require adding gstreamer1.0-plugins-good and gstreamer1.0-plugins-bad plugins as you are using v4l2h264enc in your example.
So the above line should be changed to
IMAGE_INSTALL_append += "gstreamer1.0-rtsp-server gstreamer1.0-plugins-good gstreamer1.0-plugins-bad gst-variable-rtsp-server"