Notes:
| Shell variables and pipelines | |
|---|---|
| Playback machine (receiver) | # On playback machine, set either IMX2PC or PC2IMX variables, then run the pipeline ## IMX2PC: Case where PC does the playback AUDIO_DEC_SINK="rtpamrdepay ! amrnbdec ! alsasink " VIDEO_CAPS="\"application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)H263-1998\"" VIDEO_DEC_SINK="rtph263pdepay ! ffdec_h263 ! autovideosink" ## End of IMX2PC Settings ## PC2IMX: Case where iMX does the playback AUDIO_DEC_SINK="rtpamrdepay ! mfw_amrdecoder ! alsasink " VIDEO_CAPS="\"application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)H263-1998\"" VIDEO_DEC_SINK="rtph263pdepay ! vpudec ! mfw_v4lsink " ## End of PC2IMX Settings PLAYBACK_AUDIO="udpsrc caps=\"application/x-rtp,media=(string)audio,clock-rate=(int)8000,encoding-name=(string)AMR,encoding-params=(string)1,octet-align=(string)1\" \ port=5002 ! rtpbin.recv_rtp_sink_1 \ rtpbin. ! $AUDIO_DEC_SINK \ udpsrc port=5003 ! rtpbin.recv_rtcp_sink_1 \ rtpbin.send_rtcp_src_1 ! udpsink port=5007 sync=false async=false" PLAYBACK_VIDEO="udpsrc caps=$VIDEO_CAPS port=5000 ! rtpbin.recv_rtp_sink_0 \ rtpbin. ! $VIDEO_DEC_SINK \ udpsrc port=5001 ! rtpbin.recv_rtcp_sink_0 \ rtpbin.send_rtcp_src_0 ! udpsink port=5005 sync=false async=false" PLAYBACK_AV="$PLAYBACK_VIDEO $PLAYBACK_AUDIO" # Playback pipeline gst-launch -v gstrtpbin name=rtpbin $PLAYBACK_AV |
| Streaming Machine (sender) | # On Streaming machine, set either IMX2PC or PC2IMX variables, then run the pipeline ## IMX2PC: Case where iMX does the streaming IP=x.x.x.x # IP address of the playback machine VIDEO_SRC="mfw_v4lsrc" VIDEO_ENC="vpuenc codec=h263 ! rtph263ppay " AUDIO_ENC="audiotestsrc ! amrnbenc ! rtpamrpay " ## END IMX2PC settings ## PC2IMX: Case where PC does the streaming IP=y.y.y.y # IP address of the playback machine VIDEO_SRC="v4l2src" VIDEO_ENC="ffenc_h263 ! rtph263ppay " AUDIO_ENC="audiotestsrc ! amrnbenc ! rtpamrpay " # END PC2PC settings STREAM_AUDIO="$AUDIO_ENC ! rtpbin.send_rtp_sink_1 \ rtpbin.send_rtp_src_1 ! udpsink host=$IP port=5002 \ rtpbin.send_rtcp_src_1 ! udpsink host=$IP port=5003 sync=false async=false \ udpsrc port=5007 ! rtpbin.recv_rtcp_sink_1" STREAM_VIDEO="$VIDEO_SRC ! $VIDEO_ENC ! rtpbin.send_rtp_sink_0 \ rtpbin.send_rtp_src_0 ! queue ! udpsink host=$IP port=5000 \ rtpbin.send_rtcp_src_0 ! udpsink host=$IP port=5001 sync=false async=false \ udpsrc port=5005 ! rtpbin.recv_rtcp_sink_0" STREAM_AV="$STREAM_VIDEO $STREAM_AUDIO" # Stream pipeline gst-launch -v gstrtpbin name=rtpbin $STREAM_AV |
You need to include that element, which is inside the gst-plugin-good plugin.
See RTP Streaming using gstreamer fails - gstrtpbin element missing . Appears to have been some form of conflict
Hi Leonardo,
I am trying to use above gstreamer commands with imx6 and I am getting this error - erroneous pipeline: no element "amrnbenc"
I am using Yocto 1.6. Can you tell me how to fix this ?