Author:Fourier Email:samssmarm@gmail.com
AMP:(Asymmetric Multiple Processing)
Scenario:cpu core 0 run Linux, cpu core 1 run uC/OS-II RTOS. HDMI display panel link to Linux, LCD display panel link to uC/OS-II RTOS.
Platform:
Mars Board(freesclae i.mx6 dual Coretex-A9 core, 1GB 64bit DDR3)
Panda Board(TIOMAP4460 dual Cortex-A9 core, 1GB 32bit DDR3)
Altera SoC EVMBoard(dual Cortex-A9 core, (512MB+256MB ECC) DDR3 on HPS, 512MB on FPGA)
Video Demo On Mars Board:
Youtube: http://youtu.be/yb6KC6Cf8i4
http://youtu.be/1uzrX-YZBnQ
Youku: http://v.youku.com/v_show/id_XNTMyNTAzNjky.html
AMP Port:
Linux SMP boot procedure is not mention here, For detail about the Linux SMP boot procedure please refer to the document here,http://www.linux-arm.org/LinuxBootLoader/SMPBoot.I just move the boot secondary procedure from Linux to U-boot as figure 1 in the AMP implementation, and figure2 describe the GIC relationship between two core and physical memory layout between Linux and uC/OS-II.

Figure 1

Figure 2
Display Subsystem Block on Mars Board and Panda Board:

Figure 3 imx6 display subsystem(Mars Board)

Figure 4 omap4460 display subsystem on panda board