Boot The i.mx6 dual With Linux+uC/OS-II AMP
Author:Fourier Email:samssmarm@gmail.com
AMP:(Asymmetric Multiple Processing)
Scenario:cpu core 0 run Linux, cpu core 1 run uC/OS-II RTOS. HDMI display panel link to Linux, LCD display panel link to uC/OS-II RTOS.
Platform:
Mars Board(freesclae i.mx6 dual Coretex-A9 core, 1GB 64bit DDR3)
Panda Board(TIOMAP4460 dual Cortex-A9 core, 1GB 32bit DDR3)
Altera SoC EVMBoard(dual Cortex-A9 core, (512MB+256MB ECC) DDR3 on HPS, 512MB on FPGA)
Video Demo On Mars Board:
Youtube: http://youtu.be/yb6KC6Cf8i4
Youku: http://v.youku.com/v_show/id_XNTMyNTAzNjky.html
AMP Port:
Linux SMP boot procedure is not mention here, For detail about the Linux SMP boot procedure please refer to the document here,http://www.linux-arm.org/LinuxBootLoader/SMPBoot.I just move the boot secondary procedure from Linux to U-boot as figure 1 in the AMP implementation, and figure2 describe the GIC relationship between two core and physical memory layout between Linux and uC/OS-II.
Figure 1
Figure 2
Display Subsystem Block on Mars Board and Panda Board:
Figure 3 imx6 display subsystem(Mars Board)
Figure 4 omap4460 display subsystem on panda board
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Report Inappropriate Content
hello,
thanks for illustration but how could i get the port for ucOS-II??
regards

- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Report Inappropriate Content
can u list the source code for the porting layer or the illustration about it on cortex a9 thnx in advance
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Report Inappropriate Content
Hi,
I would thank you for this demonstration.
I am a beginner to IMX6 product and I want to use two different OS as you (one for HMI and the other one for computation/control).
Is there a memory latency due to each OS tries to access the memory at the same time?
If yes do you know the how long time are needed?
Thanks for your information
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Report Inappropriate Content
Hi,
Thanks a lot for your presentation.
i have the RTOS image in ELF format. May i know how to load and execute the same in secondary cores?
my entry point is 0x30000000.
1. i have used "fatload mmc 1:1 0x30000000 rtos.elf" to load the image in U-boot console.
2. "cpu 1 release 0x30000000" but nothing works
could you please help me to solve this issue?
Thanks in advance