i.MX93 LVGL how to use PXP rendering

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX93 LVGL how to use PXP rendering

ソリューションへジャンプ
1,628件の閲覧回数
chrishoen
Contributor I

I'm trying to get the LVGL benchmark program for MX93 (LVGL ported to i.MX 93 Evaluation Kit) (https://github.com/lvgl/lv_port_nxp_imx93.git) working so that it uses the PXP gpu for rendering.

In lv_config.h, I set

#define LV_USE_DRAW_PXP 1

and get compile errors:

fatal error: fsl_cache.h: No such file or directory

which are obviously not MX93,  but for some NXP microcontroller.

Any advice on where I can go from here is appreciated.

Thanks

Chris

0 件の賞賛
返信
1 解決策
1,578件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @chrishoen!

 

According with our Linux Documentation the GPU 2D works with the PXP Module in iMX93.

The LVGL should run in the GPU 2D that is helped for PXP module.

 

Best Regards!

Chavira

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,596件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @chrishoen!

Thank you for contacting NXP Support!

 

The pxp feature is only available on iiMX RTxxx platform.

 

Best Regards!

Chavira

0 件の賞賛
返信
1,582件の閲覧回数
chrishoen
Contributor I
Hi Chavira
OK, so do any of the following lvgl selections in CMakeLists.txt: LV_USE_WAYLAND, LV_USE_SDL, LV_USE_DRM actually use the PXP?
Chris
0 件の賞賛
返信
1,579件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @chrishoen!

 

According with our Linux Documentation the GPU 2D works with the PXP Module in iMX93.

The LVGL should run in the GPU 2D that is helped for PXP module.

 

Best Regards!

Chavira

0 件の賞賛
返信