Hi, thanks for your answer,
i've allreadyu tried increasing/decrasing CMA between 512M and 256M, without success. I will try icreasing to 996 as you suggest.
when the problem occurs, cat /proc/meminfo does not show we run out of memory (i mean cma free is quite correct), so i don't think it is a cma meory issue.
I found on nxp forum a post mentionning the CONFIG_MX6_VPU_352M.
On my setup this is not activated. I am currently running a test with this config activated, and it seems it decrease the frequency of the problem.
If i understand well this option, this will increase the VDDPu and de activate the busfreq driver.
Is it something i should go further on?
Hi,
I see some issue in galcore, are you working with module galcore or driver? I can not reproduce this issue but repeat I have 4GB of RAM, maybe this is related. also please try to test the latest BSP.
Regards
Hi,
i use galcore as a module.
i've tried 6.4.3.p4.6 and 6.4.3.p4.10 version
Regards
Laurent
Hi,
correct! you may check if the driver fails please download and test the official BSP:
Regards
Hello,
Just for the top of my head, try to move the DMAhigh address to more memory o less memory and try to change the CMA to 916M, this is a memory issue the graphics app must run. I tested to run two QT app on 6.6.36 BSP and works ok without modify nothing just i have 4 GB of RAM
Regards