OPENGL ES 2.0 Sample example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OPENGL ES 2.0 Sample example

2,239 Views
deeksha
Contributor III

Hi All,

I'm trying to test Opengl Es 2.0 and OpenVG library in i.MX6 DL. So I' trying to execute sample programs in the 

/opt/imx-gpu-sdk/GLES2 and OpenVG

but I'm getting as 

WARNING: Window Size/Position values not set, setting them to Full Resolution of Primary CRT

Please help me in resolving this 

Regards,

Deeksha

0 Kudos
Reply
2 Replies

2,219 Views
deeksha
Contributor III

Hi,

There is no readme.txt available in the folder. Could you help me on the same

How can I get the source code for above sample program.

Regards,

Deeksha

0 Kudos
Reply

2,230 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello deeksha,

There is a Readme.txt in the same folder. You can follow the instruction for howto use the demo.

Regards

 

 

0 Kudos
Reply