GPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPU

3,609 Views
linhaha
Contributor I

May I ask who provided the display obtained by EGL in openVG demo of IMX RT1170  board?

0 Kudos
Reply
6 Replies

3,598 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Display for RT1170 can be found here: 5.5" LCD Panel | NXP Semiconductors

Best regards,
Omar

0 Kudos
Reply

3,582 Views
linhaha
Contributor I
I can`t understand,What is the connection between fbGetDisplay API and LCD driver?Where is fbGetDisplay implemented?
0 Kudos
Reply

3,571 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Could you please detail your question? What example, in particular, are you referring to?
The official is to ask Vivante for these materials like Vivante OpenVG API, source code, etc.

Best regards,
Omar

0 Kudos
Reply

3,547 Views
linhaha
Contributor I
Do I have to use the operating system to use the openVG API on the RT1170 board, and if so, why?
0 Kudos
Reply

3,214 Views
howardliu
Contributor II

@linhaha You have to use FreeRTOS OS. The source code of EGL isn't available. You still can use the other display panel. To use new display, you need to modify the display_support.c and .h files for new display panel.

0 Kudos
Reply

3,504 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

I suggest you consult this with Vivante to check whether the OS is strictly necessary.

Best regards,
Omar

0 Kudos
Reply