コミュニティを検索
10-14-2015
12:16 AM
1件の賞賛
Hi guys, Can anyone help me in getting a code for KEA-128 communicating with ISL29023(ambient light sensor) in I2C ?
02-16-2017
05:02 AM
Hi all, i ma trying to run I2C on kea 128 development board. the module which i am testing is I2C0 and the slave device being addressed is MPU IMU 9DOF. I have done the mandatory setting required f...
- タグ:
- kea-128
ラベル
01-25-2017
05:36 AM
Hi, I'm trying to use the header file for the kea128 I2C driver, but am getting the error "I2C Type has no member named A, C1 cannot be resolved" on every line in the header file "pI2Cx->C...
11-26-2021
02:22 PM
Hello, I am trying to add a new channel to my ADC polling. Adding this new channel to the FIFO breaks everything and I am unsure why. I am trying to measure the internal chip temperature if an I2C c...
11-15-2014
11:42 PM
1件の賞賛
I am trying to get the I2C module working on the KEA but I am having no luck with this. I can see using a logic that the SCL line goes high before the SDA line and at the end the SDA goes low b...
ラベル
12-30-2016
02:30 PM
3件の賞賛
Hello All, I am using FRDM DEV BRD KEAZ and S32DS. I need boot loader examples (using I2C, SPI, UART, CAN etc). I found KBOOT, but as I understand it doesn't support KEA devices. Where can I...
月曜日
Hi everyone: During the application of the KEAZN32 single-chip microcontroller based on LIN communication and I2C host interrupt peripheral, I encountered problems such as abnormal L...
ラベル
05-02-2017
12:07 AM
Hello, What is the slew rate requirement for input (GPIO, UART, I2C, CAN) of S9KEAZ128AMLK series micro-controller ? could not find any such information in the datasheet. Best,
08-15-2017
03:02 AM
Hi all, When the MCU is waken up from the stop mode through I2C address matching, the first transmission will be lost, i.e. no ACK is received. Is this by design for KEA...