05-28-2025
01:32 PM
1 项奖励
This document provides a step-by-step guide to building the NXP Auto Linux Yocto BSP using WSL 2 (Windows Subsystem for Linux) instead of a full virtual machine or native Linux i...
标签:
01-16-2022
09:54 PM
2 项奖励
This doc explain our Linux BSP driver and how to custom them. Contests as follows: include bsp30/32
目录 1 S32G Linux文档说明 ................................................. 2 2 创建S32G RDB2 Linux板级开发...
标签:
05-28-2025
02:36 AM
...dapt the changes, for details, it could be accessed via the following link:
https://community.nxp.com/t5/S32G-Knowledge-Base/How-to-build-older-Auto-Linux-BSPs/ta-p/1637516
(Note that the o...
标签:
11-25-2025
08:01 PM
This document explains how to enable and test Bluetooth 6LoWPAN (IPv6 over Low-power Wireless Personal Area Networks) in the i.MX Linux BSP.
Environment
i.MX Linux BSP 6.6.52...
10-10-2019
09:21 AM
8 项奖励
Hello everyone, this document will explain on how to use the UUU (Universal Update Utility) tool to flash Linux to an i.MX device (i.MX 8MM). Requirements: MX 8M Mini EVK UUU t...
01-30-2025
09:37 AM
1 项奖励
...rdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0001-gpio-pca953x-fix-pca953x_irq_bus_sync_unlock-race.patch
$ git apply ../meta-imx-frdm/meta-imx-bsp/recipes-kernel/linux/linux-imx/0002-arm64-dts-a...
08-21-2023
11:36 PM
3 项奖励
Introduction
Prior to 6.1.22_2.0.0 BSP release, Bluetooth interface are based on the tty line discipline framework, so we need to use hciattach tool to enable it in the user s...
04-20-2023
01:41 PM
3 项奖励
...nstructions below have also been uploaded to github:
https://github.com/nxp-auto-linux/linux-bsp-utils/tree/master/codeaurora_migration
However please feel free to use this article for reference a...
06-04-2025
06:32 PM
...ithub.com/nxp-auto-linux/auto_yocto_bsp -b release/bsp44.0 repo sync . nxp-setup-alb.sh -m s32g399ardb3 bitbake fsl-image-base but encountered the following build errors during the b...