eIQ Portal crashes on windows 11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eIQ Portal crashes on windows 11

ソリューションへジャンプ
7,433件の閲覧回数
alberto_alvarez
NXP Employee
NXP Employee

Hi,

 

I was trying to do some training using eIQ Portal v2.2.14 on Windows 11 but every time I try to start the training process I get this error: 

    Server encountered error: TypeError: network error

Are there compatibility issues between Windows 11 and eIQ Toolkit software? I was not able to fix this.

I also share the main.log that I get with this problem. I am using CUDA and cuDNN on my setup.

 

Thanks!!

Alberto Alvarez

0 件の賞賛
1 解決策
7,414件の閲覧回数
alberto_alvarez
NXP Employee
NXP Employee

Hi,

The problem is solved. eIQ Toolkit is compatible with Windows 11. I thought that the problem was directly caused by eIQ Portal, but I was wrong.

Downgrading cuDNN from v8.3.0 to v8.2.4 solved the problem. I am using CUDA 11.5.

Thanks!

元の投稿で解決策を見る

0 件の賞賛
1 返信
7,415件の閲覧回数
alberto_alvarez
NXP Employee
NXP Employee

Hi,

The problem is solved. eIQ Toolkit is compatible with Windows 11. I thought that the problem was directly caused by eIQ Portal, but I was wrong.

Downgrading cuDNN from v8.3.0 to v8.2.4 solved the problem. I am using CUDA 11.5.

Thanks!

0 件の賞賛