Python bindings for TF & TF-Lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Python bindings for TF & TF-Lite

Jump to solution
5,709 Views
jose_ruiz
NXP Pro Support
NXP Pro Support

Hello,
We have the need to use python 3 bindings and Keras (either Keras or tf.keras) as the front end for TensorFlow and TensorFlow Lite on i.MX8QuadXPlus. From the i.MX Linux Release Notes (L4.19.35) I can see that Hardware Accelerated eIQ Machine Learning is supported on this SoC, however, there are no further details on what features are supported for each framework (TF, TF-lite, OpenCV) and on what version. There is also no mention of the Python bindings for TF or TF-lite, are these available? On what version (2.7, <=3.6 or >=3.7)?

Is there up to date documentation regarding the supported features for each SoC?

Thank you
Jose Ruiz

joseogandoj

Labels (1)
0 Kudos
1 Solution
5,397 Views
vanessa_maegima
NXP Employee
NXP Employee

Next release will be available by the end of this month, March 31st.

Internal image at this point uses Python 3.7.

View solution in original post

3 Replies
5,397 Views
vanessa_maegima
NXP Employee
NXP Employee

Hi Jose,

In L4.19.35 TfLite supports running inference on GPU:

Screenshot from 2020-03-03 12-45-10.png

Screenshot from 2020-03-03 12-49-21 - 1.png

From Release Notes, 8QXP supports this NN acceleration:

Screenshot from 2020-03-03 12-50-08.png

Keras is currently not supported.

Python3 bindings for TfLite and ArmNN will be available in future releases.


Thanks,
Vanessa

0 Kudos
5,397 Views
jose_ruiz
NXP Pro Support
NXP Pro Support

vanessamaegima‌ Thank you very much for your detailed response. Is there an expected release date for python 3 bindings? Do you know what version of python 3 will be used (<=3.7)?

Thank you

JM

0 Kudos
5,398 Views
vanessa_maegima
NXP Employee
NXP Employee

Next release will be available by the end of this month, March 31st.

Internal image at this point uses Python 3.7.