IMX93evk zephyr RS485

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX93evk zephyr RS485

176 次查看
zefox
Contributor II

Hi,

 

I have been working on this issue for 2 days now and I am not progressing anymore. I am trying to use OSDP in Zephyr through the control_panel example. I have provided my files in the zip I attached below. 

My wiring is as follows:

zefox_0-1759829994100.png

 


I have checked that the GPIO17 is indeed multiplexed correctly. This is correct.
I have tried using pull-down resistors (10K) on the DE&/RE pin. Didn't do anything.
I have tried sending test data directly using the serial driver in Zephyr. Didn't work.

I can tell it is sending correctly because my reader is correctly receiving a message. But the DE pin always stays high. This means it won't receive anything. Which is exactly what I am observing. 

I have had this issue with the STmicroelectronics UART driver as well where the hardware-controlled DE pin had the same issue. 

How do i fix this issue

0 项奖励
回复
1 回复

149 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @zefox 

Unfortunately, this channel does not provide support to Zephyr.

 

Best regards,

Salas.

0 项奖励
回复