Resources for Zephyr modules, subsystems, and features

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Resources for Zephyr modules, subsystems, and features

Resources for Zephyr modules, subsystems, and features

If you have any questions or issues related to these resources, please Ask a new question, and the NXP support team can address it there.

Bootloaders

Zephyr includes the open-source MCUboot bootloader as a module, and makes it easy to use as a bootloader for Zephyr applications.

Inter-Processor Communication (IPC) and Multicore

Zephyr includes an IPC subsystem.  Zephyr also integrates the open-source OpenAMP framework for communication between cores using the RPMsg protocol.

LVGL graphics

Zephyr integrates LVGL as a module, provides samples, and makes it easy to use LVGL in a Zephyr app.

Networking stack

Zephyr includes a native networking stack.

 

Power Management (PM)

Zephyr includes a Power Management subsystem, supported on many NXP SOCs.

PSA and Trusted Firmware (TF-M)

Startup code and process

For portability, Zephyr manages startup code that is not included in the application.  The SOC, memory, device drivers, and some subsystems are initialized before main().

 

Return to Zephyr Knowledge Hub

No ratings
Version history
Last update:
‎12-19-2025 08:46 AM
Updated by: