zigbee serial port passthrough

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

zigbee serial port passthrough

6,198 Views
13560436802
Contributor II

zigbee(JN5169) how to implement  serial port passthrough function? use which cluster?

(如何实现串口透传功能?)

0 Kudos
Reply
8 Replies

5,663 Views
13560436802
Contributor II

Thank you for your reply.

My application like that,for example ,i  have 100 bytes data send from" STM32 A" to "STM32 B" . 

In this process,the jn5169(A) get the data from serial port and send to another jn5169(B) through the zigbee wireless. the jn5169(B) send the received data to the STM32 B through serial port at once when get the data from jn5169(A);

z.png

i have saw the zigbee cluster library user guide, but i can't find  a suitable cluster to do it;

waiting for your reply,thank you!

0 Kudos
Reply

5,663 Views
13560436802
Contributor II

Hi mario,

Thank you very much for your reply.

1. I can send fixed length array data now:

    //load payload data into APDU

pastedImage_8.png

2.I have anther question about  how to set the data format when send the indefinite length data?

pastedImage_9.png

0 Kudos
Reply

5,663 Views
quanjunzhang
Contributor III

Hi Dylan,

Can you tell me how to receive a fixed amount of data?

Thanks vary much.

capture_20190702225457684.bmp

Regards,

Zhang

0 Kudos
Reply

5,663 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dylan,

Did you check the parameters?

hAPduInst Handle of the APDU instance to write the data into

u32Pos The starting position (least significant byte) of the data within the APDU instance

*szFormat Format string of the data:

  • b 8-bit byte
  • h 16-bit half-word (short integer)
  • w 32-bit word l 64-bit long-word (long integer)
  • a\xnn nn (hex) bytes of data (array)
  • p\xnnnn (hex) bytes of packing ... Variable list of data values described by the format string

Note that the compiler will not correctly interpret the format string “a\xnnb” for a data array followed by a single byte, e.g. “a\x0ab”. In this case, to ensure that the ‘b’ (for byte) is not interpreted as a hex value, use the format “a\xnn” “b”, e.g. “a\x0a” “b”.

Regards,

Mario

0 Kudos
Reply

5,663 Views
13560436802
Contributor II

Hi Mario,

I have another question about receiving;

For example, if A device send data to the B device. the B device how to get the data in the application layer?

pastedImage_1.png

0 Kudos
Reply

5,663 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dylan,

Please look at the PDUM_pvAPduInstanceGetPayload

https://www.nxp.com/docs/en/user-guide/JN-UG-3116.pdf 

Regards,

Mario

0 Kudos
Reply

5,663 Views
13560436802
Contributor II

Hi,Mario,

I saw it,But i still don't understand how to send  indefinite length data;

Could you give me an example?

0 Kudos
Reply

5,663 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dylan,

I am not sure, what is the final application that you want.

You can look at the ZigBee Cluster Library User Guide document and look at one cluster that could be equal for your application, or you can create a custom cluster.

Regards,

Mario

0 Kudos
Reply