zigbee communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,998件の閲覧回数
syed_idris
Contributor III

Hi all,

We are currently working on Kinetis KW40, as zigbee in already there in this microccontroller.

1.How to make zigbee communication of this controller with another zigbee module?

2.Where (in which register) the recieved data of zigbee is stored?

Thanks,

Syed_Idris

1 解決策
5,377件の閲覧回数
EarlOrlando
Senior Contributor II

Hello,

As I said, this MCU is not still supported for the BeeStack (NXP's ZigBee Stack). If you HAVE to use ZigBee you need to move to other MCU as I said in my last answer. The MKW40Z is only supported by SMAC, MAC (802.15.4) and BLE stacks.

Depending on your requirements I can recommend you one of those stacks to start developing.

The stacks I mention are included in the KW40Z Connectivity Software which is only supported by IAR. If you want to use KDS and the Kinetis SDK you must build your own application (as any other MCU). I don't recommend this option.

Best regards,

Earl.

元の投稿で解決策を見る

5 返答(返信)
5,377件の閲覧回数
EarlOrlando
Senior Contributor II

Hello,

The BeeStack (NXP's ZigBee Stack) is a full software stack which enables all the ZigBee protocol in the Kinetis devices. Unfortunately, The KW40Z devices are not supported in the latest BeeStack 5.0.0 codebase. This release supports the KL4xZ + MCR20A transceiver, K6xF + MCR20A transceiver and MKW2xD MCUS.

The MKW40Z Connectivity Software​ supports this device and it includes the SMAC, MAC and BLE stacks.

Also, if you have two MK2xD boards I recommend you to run this guide to get started with our BeeStack.

Running a demo with BeeKit (802.15.4 MAC, SMAC and ZigBee BeeStack)

Best regards,

Earl.

0 件の賞賛
返信
5,377件の閲覧回数
syed_idris
Contributor III

We are having USB-KW40 and programming it through KDS 3.0.0 (without OpenSDA)

We want to know how the zigbee of this KW40 will communicate to another zigbee module (which is separate).

which component should we select from component library of KDS 3.0.0 If we want

- to establish a communication ,

- to send/receive the data packets

- to know the indication (acknowledgment) of sent/received data packet,

what steps you recommend us to take?

Syed_Idris

0 件の賞賛
返信
5,377件の閲覧回数
EarlOrlando
Senior Contributor II

Hello,

As I said, this MCU is not still supported for the BeeStack (NXP's ZigBee Stack). If you HAVE to use ZigBee you need to move to other MCU as I said in my last answer. The MKW40Z is only supported by SMAC, MAC (802.15.4) and BLE stacks.

Depending on your requirements I can recommend you one of those stacks to start developing.

The stacks I mention are included in the KW40Z Connectivity Software which is only supported by IAR. If you want to use KDS and the Kinetis SDK you must build your own application (as any other MCU). I don't recommend this option.

Best regards,

Earl.

5,376件の閲覧回数
rafaeltoledo
Contributor III

Is there any plans to support the Bluetooth stack by using the KDS and KSDK?

0 件の賞賛
返信
5,377件の閲覧回数
EarlOrlando
Senior Contributor II

Hello,

Maybe this message is useful for you:

Re: Router example for KW40Z/KW20Z

Earl.

0 件の賞賛
返信