Router example for KW40Z/KW20Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Router example for KW40Z/KW20Z

3,851 Views
kedarikrishna
Contributor I

After so many choices we arrived at KW40Z/KW20Z for our product. When started development, we found that there are example projects for Coordinator and end device but not router.

As  we are having product feature requirement of designing mesh network where device form mesh network .

So we are expecting any suggestion, discussion  or help to achieve the same (Zigbee Mesh network with KW40Z/KW20Z).

Labels (1)
0 Kudos
Reply
2 Replies

2,846 Views
TudorS_
NXP Employee
NXP Employee

Hello.

The KW40Z/KW20Z codebases do not include ZigBee stack support. They only have IEEE 802.15.4 MAC/PHY libraries.

Since KW40Z/KW20Z is an ARM Cortex M0+ based wireless microcontroller, you could explore leveraging the ZigBee libraries from the Kinetis BeeStack ZigBee Protocol Stack package for the MCR20A wireless transceiver and the KL46Z microcontroller (also Cortex M0+). The IEEE 802.15.4 MAC has a common API for the two hardware solutions.

The MCR20A/KL46Z Kinetis ZigBee Protocol Stack software package can be downloaded from: https://www.nxp.com/webapp/Download?colCode=KINETIS-BEESTACK&appType=license&location=null&fpsp=1&WT...http://www.nxp.com/products/interface-and-connectivity/wireless-connectivity/2.4-ghz-wireless-soluti...

0 Kudos
Reply

2,846 Views
EarlOrlando
Senior Contributor II

Hello Kedari Krishna,

Could you please specify what coordinator and end device examples you found?

Best regards,

Earl Ramírez.

0 Kudos
Reply