why i cannot upgrade the PN5180's firmware?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

why i cannot upgrade the PN5180's firmware?

跳至解决方案
9,258 次查看
andy_Musk
Contributor III

why i cannot upgrade the PN5180's firmware?

 

 

[2022.01.27 20:01:33]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while writing to COM6
[2022.01.27 20:01:33]:ERROR:BoardConnectionViewModel:Secure Firmware Upgrade Failed. Status=BAL,IO_TIMEOUT

 

 

0 项奖励
回复
1 解答
9,167 次查看
andy_Musk
Contributor III

xqhrs232_andy_0-1644418136195.png

the bin file run in LPC1769 mcu is C:\nxp\NxpNfcCockpit_v6.3.0.0\ABENDToVCOM\fw\lpc_main.bin

and i can read the M1 card's UUID.  

why i cannot upgrade the PN5180's firmware?

在原帖中查看解决方案

0 项奖励
回复
28 回复数
2,263 次查看
danielchen
NXP TechSupport
NXP TechSupport

 

AN11744 is for PNEV5180 board, as below.  but it is different from yours

danielchen_0-1644420250530.png

 

0 项奖励
回复
2,241 次查看
andy_Musk
Contributor III

my PN5180 board just copy from PNEV5180!!! the communicate connection with PN5180  is the same to 

NXP.s PNEV5180!!!

0 项奖励
回复
2,239 次查看
andy_Musk
Contributor III

how to use BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin file ?

how to burn the bin file to LPC1769?

标记 (1)
0 项奖励
回复
2,199 次查看
danielchen
NXP TechSupport
NXP TechSupport

 

Please use GUI Flash tool in MCUXpresso IDE. see below picture

danielchen_0-1644420835672.png

 

 

 

 

0 项奖励
回复
2,178 次查看
andy_Musk
Contributor III

can i use Flash Magic  to burn the LPC1769  MCU?

but the Flash Magic need use hex format file.  how to convert the bin file to hex file ?

 

xqhrs232_andy_0-1644421483742.png

 

0 项奖励
回复
2,178 次查看
andy_Musk
Contributor III

i have not install  MCUXpresso IDE.  and i have not the LPClink  JTAG tool.

what can  i do ?

0 项奖励
回复
2,130 次查看
danielchen
NXP TechSupport
NXP TechSupport
0 项奖励
回复
9,168 次查看
andy_Musk
Contributor III

xqhrs232_andy_0-1644418136195.png

the bin file run in LPC1769 mcu is C:\nxp\NxpNfcCockpit_v6.3.0.0\ABENDToVCOM\fw\lpc_main.bin

and i can read the M1 card's UUID.  

why i cannot upgrade the PN5180's firmware?

0 项奖励
回复