why i cannot upgrade the PN5180's firmware?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why i cannot upgrade the PN5180's firmware?

Jump to solution
9,301 Views
andy_Musk
Contributor III

why i cannot upgrade the PN5180's firmware?

 

 

[2022.01.27 20:01:33]:FATAL_ERROR:UcVcomBalDelegate:Timeout Error while writing to COM6
[2022.01.27 20:01:33]:ERROR:BoardConnectionViewModel:Secure Firmware Upgrade Failed. Status=BAL,IO_TIMEOUT

 

 

0 Kudos
Reply
1 Solution
9,210 Views
andy_Musk
Contributor III

xqhrs232_andy_0-1644418136195.png

the bin file run in LPC1769 mcu is C:\nxp\NxpNfcCockpit_v6.3.0.0\ABENDToVCOM\fw\lpc_main.bin

and i can read the M1 card's UUID.  

why i cannot upgrade the PN5180's firmware?

View solution in original post

0 Kudos
Reply
28 Replies
2,276 Views
danielchen
NXP TechSupport
NXP TechSupport

 

AN11744 is for PNEV5180 board, as below.  but it is different from yours

danielchen_0-1644420250530.png

 

0 Kudos
Reply
2,254 Views
andy_Musk
Contributor III

my PN5180 board just copy from PNEV5180!!! the communicate connection with PN5180  is the same to 

NXP.s PNEV5180!!!

0 Kudos
Reply
2,252 Views
andy_Musk
Contributor III

how to use BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin file ?

how to burn the bin file to LPC1769?

Tags (1)
0 Kudos
Reply
2,212 Views
danielchen
NXP TechSupport
NXP TechSupport

 

Please use GUI Flash tool in MCUXpresso IDE. see below picture

danielchen_0-1644420835672.png

 

 

 

 

0 Kudos
Reply
2,191 Views
andy_Musk
Contributor III

can i use Flash Magic  to burn the LPC1769  MCU?

but the Flash Magic need use hex format file.  how to convert the bin file to hex file ?

 

xqhrs232_andy_0-1644421483742.png

 

0 Kudos
Reply
2,191 Views
andy_Musk
Contributor III

i have not install  MCUXpresso IDE.  and i have not the LPClink  JTAG tool.

what can  i do ?

0 Kudos
Reply
2,143 Views
danielchen
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
9,211 Views
andy_Musk
Contributor III

xqhrs232_andy_0-1644418136195.png

the bin file run in LPC1769 mcu is C:\nxp\NxpNfcCockpit_v6.3.0.0\ABENDToVCOM\fw\lpc_main.bin

and i can read the M1 card's UUID.  

why i cannot upgrade the PN5180's firmware?

0 Kudos
Reply